What cameras are compatible with the BHP SDK?

The following cameras series are compatible with BHP SDK:

SC6100, SC6200, SC6700, SC6800, A6600, A6700, A8200, A8300, X6800, X6900, X8500, RS6700, RS6800, RS8200, RS8300

 

The following cameras are NOT compatible with BHP SDK.

A2600sc and legacy SC8000 (sometimes called the SC8100)

Legacy SC4000/SC6000 (aka Cumulus)

Back to top