What is the ThermoVision Condition Monitor?

What is the ThermoVision Condition Monitor?

The ThermoVision Condition Monitor, also known as the TV CM, is a hardware and software system that can be used for simple condition monitor applications where the following are needed:

  • Alarms based on temperature.
  • Recorded video associated with alarms.
  • Live video.
  • Up to nine cameras support.
  • Graphical representation of the temperature data.

 

How many cameras can I connect to the TV CM?

You can have a maximum of nine cameras connected.

Which cameras are supported?

The FLIR A310, A310f, A310ex, and AX8. The FLIR A310pt is not supported.

Can I modify the program?

Yes, development software is included.

Do I need the software IR Monitor?

Yes, you still need IR Monitor, but only for adding areas and spots. The alarms should not be handled by IR Monitor. The alarms are handled by the TV CM.

Back to top