Why do I get a "Disk is Full" error message when I'm trying to save my report? I know that there is enough room left on the hard drive.

This is caused when the report can not find the template it is based on.

For Reporter 7 this can be solved by installing the SR-4 patch and enabling the "Trust access to visual basic projects" in the security dialog in Word or by making the template accessible to the document by placing the template in a shared folder.
For users of Microsoft Office 2000  and Reporter 7 it should suffice to just install the SR-4 patch.
ThermaCAM Reporter 7 SR-4 patch

For users of Reporter 8: 

To turn on the Trust access to Visual Basic Projects (Microsoft Office Word XP/2003)

  1. On the Tools menu, point to Macro, and then click Security.
  2. On the Trusted Sources tab, select the Trust access to Visual Basic Project check box.
Back to top