The reason for this could be an issue with the IP address. If the GenICam parameter GevPersistentIPAddress is set to a value that differs from the true IP address of the device, this error might occur. To fix this, simply change the GenICam parameter GevPersistentIPAddress to 0.0.0.0 or the true IP address of the device.
The GenICam parameter GevCurrentIPConfigurationPersistentIP could also be set to false to solve this issue.