Revolutionary FLIR MUVE C360 Drone-Mounted Gas Monitor Provides Faster, Safer Way to Remotely Sense Gas and Chemical Incidents

ARLINGTON, Va., September 24, 2019 ― FLIR Systems, Inc. (NASDAQ: FLIR) today announced the FLIR MUVE C360, the industry’s first multi-gas detector specifically built for unmanned aerial systems (UAS).     

The MUVE C360 will transform how emergency response teams approach chemical, industrial, or environmental incidents by providing a new level of safety, dramatically reducing time to action, and delivering a more complete assessment in situations where every second counts. The C360 is currently compatible with the DJI Matrice 210 UAS platform.

Before putting the health and safety of response teams at risk, drone pilots will be able to fly the new MUVE C360 into a scene for initial assessment. The C360 houses a photoionization detector, plus a suite of advanced electrochemical sensors that provide real-time continuous monitoring of chemical hazards such as chlorine, carbon monoxide, and other combustible gases. This capability will enable emergency response teams to assess situations remotely and select the proper personal protective equipment. Fire crews will be able to monitor air quality surrounding active scenes before entry, and industrial experts can perform inspections in hard-to-reach areas with relative ease.

The MUVE C360 will allow operators to understand the flow of hazardous vapors both at the source and in the air. It bypasses difficult terrain and enables response teams to quickly draw a perimeter and map known hazards, while preset alarm thresholds help scene commanders or security operators make quick decisions.

“First responders are constantly seeking better and safer ways to do their jobs, and from the moment the FLIR MUVE C360 arrives in the market, the chemical and gas monitoring process will change forever,” said Jeff Frank, senior vice president at FLIR. “In the time it normally takes first responders to don proper equipment, the C360 has already arrived on scene, tested samples, and located the source of a hazard.  

“With greater accessibility to drone technology than ever before, the purpose-built MUVE C360 will provide response teams with improved situational awareness that can help save lives and livelihoods,” Frank added.   

FLIR is also introducing FLIR VueLink™, a pilot flight application that provides drone operators a plug-and-play interface to the MUVE C360.  The app also includes advanced flight-control and interface with the FLIR Cloud.   

The MUVE C360 and VueLink will be available in the fourth quarter of 2019. To learn more, visit www.flir.com/C360.  

                                                    -###-

About FLIR Systems, Inc.

Founded in 1978, FLIR Systems is a world-leading industrial technology company focused on intelligent sensing solutions for defense, industrial, and commercial applications. FLIR Systems’ vision is to be “The World’s Sixth Sense,” creating technologies to help professionals make more informed decisions that save lives and livelihoods. For more information, please visitwww.flir.com and follow @flir.

Articles connexes

Article

Introducing FLIR DELTA - Season 2: The Podcast Series

Read more
Actualités sur les produits

FLIR annonce la sortie du logiciel de gestion de vol des drones DroneSense-FLIR Edition

Read more
Back to top