Flir iXX and RocketPlan: Bringing Thermal Intelligence Directly into Restoration Workflows for Faster Payouts

Thermal imaging has long been a core tool in property restoration, helping professionals uncover hidden moisture, temperature anomalies, and structural issues that aren’t visible to the naked eye. As restoration work becomes increasingly digital, the real value of thermal data lies not just in capture, but in how easily that data flows into documentation, reporting, and decision-making, supporting smoother projects and helping teams get paid faster.

Flir continues to expand its ecosystem of app‑connected solutions through strategic partnerships that bring thermal intelligence closer to daily workflows. One example is the integration between Flir iXX cameras and RocketPlan, a restoration workflow platform designed to connect field activities with office processes.

Moving Thermal Imaging into the Workflow

While thermal imaging is widely used, many restoration teams still face inefficiencies, including images stored separately from job records, manual file transfers, and limited context when reviewing inspections later. These gaps create unnecessary administrative work and slow down reporting for clients and insurers.

The integration of Flir iXX with RocketPlan addresses these challenges by making thermal imagery a native part of the restoration workflow. With this integration, thermal images captured in the field are automatically associated with the correct job, location, and timestamp. They appear alongside photos, notes, and reports, without the need for manual uploads or file management. The result is a more connected process, from inspection through documentation.

Practical Benefits for Restoration Teams

By embedding thermal data directly into RocketPlan workflows, restoration professionals gain:

  • Streamlined field-to-office handoff, with a single, consistent source of project data
  • Clearer documentation and reporting, supporting communication with clients, insurers, and internal teams
  • Faster, more confident decisions, driven by accurate thermal insight in full project context
  • Reduced administrative effort, allowing teams to focus on remediation rather than paperwork
  • Greater consistency across teams and locations, supporting standardized processes at scale, and helping organizations get paid faster.

Designed for Connected Workflows

Flir iXX cameras are built for mobile, app‑connected environments. Their portability, image quality, and ease of use make them a strong fit for professionals who need reliable thermal insight without disrupting jobsite efficiency.

The iXX-Series serves as the natural flagship mobile thermal integration; the platform also supports Flir One, Flir Edge, and Flir MR277, giving restoration teams flexibility across imaging and measurement tools.

Expanding the Role of Thermal Imaging

This integration reflects a broader shift in restoration work: from standalone inspections to connected workflows that improve collaboration, efficiency, and data clarity.

By bringing Flir iXX imagery directly into RocketPlan workflows, restoration professionals can turn thermal insight into actionable results, supporting faster decisions, clearer documentation, and more efficient projects from start to finish.

Back to top