Why QOGI Matters: Improving Safety and Operations in Difficult-to-Access Areas


This article is part of our ongoing series looking at why adding quantitative OGI (QOGI) to a leak detection and repair (LDAR) regimen is critical to improving efficiency and safety, strengthening compliance, and optimizing methane monitoring programs.
Safety has always been at the core of leak detection and repair (LDAR) programs. Whether in upstream oil and gas operations, refining environments, or chemical manufacturing, identifying and addressing gas leaks is critical not only for environmental compliance but also for protecting personnel and ensuring safe operations.
However, many of the most challenging safety risks in LDAR do not come from the leaks themselves — but from the process of detecting them. Inspecting equipment often requires technicians to work at height, enter confined spaces, or approach pressurized systems operating under hazardous conditions.
As facilities become more complex and regulatory requirements increase, operators are looking for ways to reduce these risks without compromising inspection coverage. This is where Quantitative Optical Gas Imaging (QOGI) provides a meaningful advantage.
By enabling remote detection and quantification of gas leaks, QOGI fundamentally changes how inspections are performed—improving both safety outcomes and operational efficiency, especially in difficult-to-access areas.
Traditional leak detection methods often rely on contact-based measurement techniques. In these workflows, inspectors use handheld instruments to measure gas concentrations directly at potential leak points.
While effective in many scenarios, this approach introduces several inherent safety risks:
These risks are amplified when facilities contain thousands of components spread across large or complex layouts. Even with strong safety protocols, physically accessing each inspection point increases the likelihood of incidents.
In addition, traditional methods can limit visibility. Inspectors are often focused on individual components, making it difficult to observe larger system behavior or detect leaks that originate outside immediate reach.
Quantitative Optical Gas Imaging builds on the principles of optical gas imaging by allowing operators to detect and quantify emissions from a distance. Like standard OGI, QOGI uses specialized infrared cameras to visualize gases such as methane and volatile organic compounds (VOCs), which absorb infrared radiation at specific wavelengths. When a gas plume is present, it creates a visible contrast against the background, appearing as a moving cloud in the camera view.
The key safety advantage is that this inspection is non-contact.
Instead of placing a probe directly on each component, inspectors can scan entire systems from several feet — or even tens of feet — away. This reduces the need to:
By increasing the distance between personnel and potential hazards, QOGI directly lowers exposure risk. In practical terms, this means inspectors can perform more of their work from safer ground-level positions or designated observation points.

Many of the most critical emissions — and safety risks — occur in areas that are difficult to access using traditional methods. These include:
In these environments, traditional inspection methods often require additional equipment (lifts, scaffolding) or specialized permits (confined space entry), increasing both time and risk.
QOGI changes this dynamic by enabling remote inspection.
This ability to monitor difficult-to-access areas without direct contact significantly reduces the operational burden of maintaining safe inspection practices.
Gas leaks are not just an environmental concern — they can pose serious health and safety risks.
Methane and VOCs can displace oxygen in confined spaces, contribute to explosive atmospheres, or expose workers to harmful chemicals. In traditional LDAR workflows, inspectors may need to approach these leaks closely to confirm their presence.
QOGI reduces this exposure.
Because leaks can be detected visually from a distance, inspectors can:
This is particularly important in scenarios involving large or unexpected releases. For example, a significant leak detected using QOGI can be assessed remotely, allowing teams to evaluate the situation before taking corrective action.
Field experience has shown that OGI technology helps operators quickly locate leaks while reducing the risk of gas exposure for staff during routine inspections. With QOGI, these same users can quickly understand the severity of the emissions while remaining safe.
While traditional OGI improves safety by enabling remote detection, QOGI adds another layer of value: quantification.
By estimating the size of a leak in real time, QOGI helps operators better understand the potential risk associated with each emission event.
This supports more informed decisions, such as:
In high-risk environments, having this information at the point of detection can be critical. Instead of relying on assumptions or delayed measurements, QOGI provides immediate insight into the scale of the problem.
This reduces uncertainty and enables teams to respond more effectively — without unnecessary exposure or delay.
Another safety benefit of QOGI is improved situational awareness.
Traditional methods focus on individual components, often limiting the inspector’s view to a single point at a time. In contrast, OGI-based technologies provide a broader perspective, allowing operators to observe how emissions behave across an entire system.
This can reveal:
Studies of OGI use in industrial settings have shown that visualizing leaks directly can improve coordination between environmental, safety, and operations teams, leading to better overall risk management and reduced downtime following leak incidents.
By making emissions visible, QOGI helps bridge the gap between detection and action—ensuring that all stakeholders have a clear understanding of the situation.
In addition to handheld inspections, QOGI technologies are increasingly being integrated into continuous monitoring systems.
Fixed or automated OGI solutions can monitor critical assets in real time, providing:
This approach enhances safety by detecting issues as they happen, rather than waiting for the next scheduled survey.
In environments where conditions can change rapidly, continuous monitoring provides an added layer of protection — allowing operators to respond quickly before small issues escalate into safety incidents.
Regulatory frameworks are evolving to emphasize not only emissions reduction but also safe and verifiable inspection practices.
The U.S. Environmental Protection Agency (EPA), for example, has established detailed requirements for the use of optical gas imaging in LDAR programs, including training, performance standards, and documentation protocols.
These requirements reinforce the importance of:
QOGI supports these objectives by providing both visual and quantitative data, improving transparency and traceability in inspection workflows.
At the same time, the ability to reduce physical access requirements aligns with broader safety goals — helping operators meet regulatory expectations while protecting their workforce.
Safety and efficiency are often closely linked. When inspections can be performed more safely, they can also be performed more consistently and with fewer disruptions to operations.
QOGI contributes to this balance by:
These advantages make QOGI a valuable tool for modern LDAR programs — especially in facilities where safety constraints can limit inspection frequency or coverage.
As discussed in earlier articles in this series, QOGI improves efficiency and supports regulatory compliance. Its role in enhancing safety builds on these benefits, creating a more comprehensive approach to emissions monitoring.
In the next article, we will explore how QOGI supports future-proofing LDAR programs, helping operators transition toward more advanced approaches such as leak detection and quantification (LDAQ).