What do CAT Ratings Mean?

Comprehending Safety Ratings for Electrical Tools, Test and Measurement Equipment 

The International Electrotechnical Commission (IECdevelops and distributes international standards for electrical technologies, including for devices used to identify, test and measure live electrical circuits.  

Known as thmeasurement category, this method of classification examines the total potential continuous energy available at any point within a circuit, including the potential for transient voltages that can spike voltages well beyond normal levels. Transient voltages can be caused by lightning strikes, arching or other naturally occurring electrical phenomena, which can pose significant danger to personnel working on or around electrical equipment, from fixing a copy machine through to examining power utility infrastructure.  

The measurement categories are divided into four parts, known individually as category (CAT) ratingsCAT I, CAT II, CAT III and CAT IV. Understanding what each of these categories means is vital to choosing the right equipment for the job to avoid exposure to unnecessary risk. In short, the rating system will inform anyone working with electrical equipment about the right tool for a job, whether a basic multimeter will suffice through to selecting the right devices for industrial utility infrastructure inspection  

Understanding Voltage Ratings  

CAT-Web-Article_Cross-Sectional_Industrial-1200x628 010821.jpg

In the CAT ratings system, the roman numerals, (i.e. I through IV) refer to the location of a circuit in relation to the power source, defined in terms of the total potential transient voltage danger  

  • CAT I describes secondary circuits not intended to be connected to the mains electricity supply, such as electronicsincluding a typical laptop PC, and circuits powered by regulated low voltage sources. 
  • CAT II is defined as local-level electrical distribution, such as standard mains socket and plug-in loads. This category includes household appliances, such as washing machinesand portable plug-in power tools.  
  • CAT III references a building’s electrical installations, including circuit-breakers, wiring, switches and industrial equipment 
  • CAT IV involves the source of the low-voltage power installation, essentially the power grid infrastructure, such as underground utility vaults or outdoor power lines 

However, determining the appropriate voltage category is only half the story. Simply matching the presumed voltage to the test and measurement device will also not provide adequate safety assurance. Failed electrical units can experience impulse or transient voltages on the order of many times a particular electrical tool’s rating. For example, a line may normally have a voltage of 120 or 240, but a lightning strikes can create transient voltage, perhaps several thousand volts, that can cause a short circuit and arcing that may severely injure personnel testing the power infrastructure with inadequate equipment  

In essence, not only must the tool have the appropriate CAT rating for the application, the device must also have a voltage rating higher than the maximum voltage of the given environment to withstand potentially dangerous surges in voltage.  

Thankfully, IEC supplies a quick-reference chart to determine whether or not a given electrical tool is appropriate for the task at hand.  

Rated Voltage 

IEC 61010-1 

2nd Edition 

UL 61010B-1 
(UL 31111-1) 

 

CAT IV 

CATIII 

CAT II 

CATIII 

CAT II 

CAT I 

150V 

4000V 

2500V 

1500V 

2500V 

1500V 

800V 

300V 

6000V 

4000V 

2500V 

4000V 

2500V 

1500V 

600V 

8000V 

6000V 

4000V 

6000V 

4000V 

2500V 

1,000V 

12kV 

8000V 

6000V 

8000V 

6000V 

4000V 

Resistance 

2-ohms 

 2-ohms 

12-ohms 

 2-ohms 

12-ohms 

30-ohms 

Matching the Right Electrical Tools for the Job  

If a given specification requires a tool to be rated for CAT III 600V and CAT II 1000V, then the module can withstand up to 6000V of impulse or transient voltage. This type of specification would additionally inform the user that the device must not be used with Mains CAT IIcircuits with the potential for voltage to rise above 6000V. Conversely, the tool or device rated in this manner should not be used with CAT IV circuits under any circumstances, even if a particular scenario does not require more than 6000V. 

Take the FLIR VS290-32 videoscope, primarily designed to inspect hard-to-reach underground utility vaults. The device offers thermal imaging, visible imaging or both, combined through a process called MSX, all on the end of a flexible probe with a rectangular tip. This device features a CAT IV 600V rating. Therefore, it’s ideal for inspecting utility power equipment for potential faults (such as underground utility vaults) as long as the transient or impulse voltage will not climb above 8000V.  

Ultimately, the purpose of the CAT rating system is to provide a quick and easy-to-understand method for selecting the right tool for the job, to know if a given tool is designed for a particular application/scenario or not. A quick check adds an additional level of safetyhelping to prevent serious injury or even death that could result from electrocution, fires or explosions 

When exploring FLIR multimetersclamp meters and other electrical test and measurement equipment, check the safety ratings within each products specifications to ensure that a particular device matches the planned usage scenarios.

Related articles

Choosing a Camera

What Is the Right Handheld Thermal Camera for You?

Read more
Fundamentals

Top 5 Mistakes That New Thermographers Make

Read more
Back to top