New Aerial Solar Farm Inspection Takes Off for Wesii

Wesii is an Italian provider of aerial thermography inspections which specialises in aerial inspections and the AI-based diagnosis of photovoltaic (PV) panels for the solar farm industry.

The company recently launched a new aerial inspection system for solar arrays using the latest in thermal imaging technology. By combining the high-resolution FLIR A8580 MWIR thermal camera and cooled sensor with the SmartBay© multi-sensor aeroplane platform from DigiSky, it has replaced slow, low-altitude drone inspections with an aeroplane-based system capable of inspecting as many solar panels in a single day as one drone can inspect in a week.  

Wesii can now offer its customers more cost-effective inspection flights, accurately inspecting large numbers of panels quickly, even at lower irradiance, and with far greater data consistency.

Faster, cost-effective aeroplane thermal imaging replaces drones

“The benefits of aerial inspections by aeroplane are very clear,” said Pietro Salvagno, remote sensing engineer at Wesii. “The most obvious benefit is that, with an aeroplane, you can go much higher than with a drone—up to 300 metres—and thus cover a much larger area in much less time. Up until recently, we thought that we wouldn’t be able to collect high-quality thermal data from such heights. But with Teledyne FLIR’s thermal imaging cameras, we discovered that it’s perfectly possible to collect accurate data from an aeroplane.”

Compact, high-resolution thermal imaging

Wesii needed a reliable integration partner to turn this new idea into reality - and found one in the Italian aeronautic engineering specialist DigiSky. Its SmartBay system can carry up to three different sensors on an aeroplane wing simultaneously and comes equipped with its own mission computer that automatically manages all remote sensing activities during inspection flights.

Wesii and DigiSky needed a high-resolution, high-sensitivity thermal camera with a cooled sensor, capable of precise PV analysis, while being compact enough for use on the SmartBay system. The FLIR A8580 MWIR camera with 1.3 MP resolution was the ideal solution.

“We looked at resolution, sensitivity, focal lens options, and integration possibilities, and the Teledyne FLIR A8580 offered the most interesting feature combination and capabilities to perform this task,” said Pietro Salvagno.

Accurate detection of PV defects

Wesii now uses the FLIR A8580 to detect a wide range of anomalies in PV panels. The company has developed in-house Artificial Intelligence (AI) algorithms for the categorisation and classification of defects to provide valuable reports of inspected assets. Both classification (single hot spot, multiple hot spots, diode defect, extended and string) and severity (the difference between the panel’s operating temperature and the thermal anomaly temperature) are taken into account. These findings are then combined with visual inspections, also connected to the SmartBay© system. 

“With the FLIR A8580 mounted on the SmartBay system, we can cover solar assets worth 300 megawatts per day, which would typically take an entire week using a drone,” says Salvagno. “The spatial resolution of the A8580 allows us to identify anomalies with more accuracy, and detect narrower temperature differences, so we can be even more confident about the quality of our data.”

Greater freedom to plan inspections

And there’s yet another important benefit of using a cooled camera such as the FLIR A8580. While the accuracy of an uncooled camera can decrease due to external conditions and requires a high solar irradiance (over 600 W/m2), a cooled camera can allow for a lower irradiance (400 W/m2) while still collecting accurate results.

“The Teledyne FLIR camera offers us much more freedom because we can plan inspection flights even in conditions that would be unacceptable for standard drone inspections,” said Salvagno. “In addition, we can maintain the same irradiance values throughout the entire inspection, because we can capture data in a much shorter time frame. This gives us much more data consistency, and it allows us to better compare data of different inspections.”

The future of aerial inspection

With aeroplane-based inspections, there’s no need for the onerous health and safety documentation required of drone inspections, making the planning process far more straightforward. There’s no need for in-field personnel, unlike a drone flight where the technician must be in direct line of sight. And above all, it can cover larger areas in less time than a drone, making it far more cost-effective.

Thanks to its experience working with Teledyne FLIR, Wesii is planning to shift its future focus to aeroplane-based thermography inspections.

“The feedback about the aeroplane-based approach and the Teledyne FLIR camera has been amazing,” said Mauro Migliazzi, Wesii CEO & Founder. “Many of our customers were amazed by the thermal detail and did not believe that the thermal data was coming from an aeroplane-conducted inspection. This only confirms that aeroplane inspections are the future not only for Wesii but also for the Industry.”

 

Artículos relacionados

Historia de la aplicación

El Battery Innovation Centre (Centro de Innovación de Baterías) utiliza imágenes térmicas de alta velocidad para pruebas de baterías abusivas

Read more
Historia de la aplicación

A Shot at Space: Validating Rocket Integrity With Thermal Imaging

Read more
Caso práctico

Una cámara FLIR de alta resolución pone la ciencia en la pista de carreras

Read more
Back to top