Preventing Fire and Electrical Risks in Food and Beverage Facilities


Fires and electrical issues in food and beverage facilities rarely start suddenly. They build over time, hidden inside panels, ovens, fryers, and busy production areas.
The challenge is how quickly those small issues escalate. By the time traditional systems detect a problem, the damage may already be too severe, leading to downtime, asset loss, and spoiled stock.
Thermal imaging changes that timeline; in controlled trials, it has achieved 100% fire identification with zero false alarms, detecting flame signatures the moment they appear. In food and beverage environments filled with heat, steam, and constant activity, that level of accuracy allows teams to act earlier, when risks are still manageable.
Electrical systems power nearly every part of a food and beverage operation, from processing lines and refrigeration to packaging, storage, and distribution. A fault in a single panel or switchgear can bring production to a halt, trigger equipment failure, and disrupt schedules.
Often, the first warning is subtle. A temperature rise of just 10 to 30°C inside a panel can signal loose connections, overloads, or ageing components.
These changes are easy to miss.
Most facilities rely on periodic thermal inspections to stay compliant with standards such as NFPA 70B. Those checks are important, but they only show what is happening at a single point in time. The reality is that risk does not follow a schedule. It builds between inspections, during peak demand, or late at night in unattended rooms.
In many cases, these electrical faults are the starting point for fires, making early detection critical for both electrical safety and fire prevention.

Thermal monitoring systems provide continuous visibility of temperature changes in electrical panels and equipment rooms.
With 24/7 monitoring, abnormal heat patterns can be identified as they develop, rather than waiting for a scheduled inspection or fault condition. This allows teams to act earlier and reduce the likelihood of failure or fire.
Maintenance teams can pinpoint overheating components early, track temperature trends over time, and investigate issues before they escalate, allowing maintenance to be planned rather than reactive.
The result is safer operations and more predictable uptime, with fewer unexpected failures.
See all of our Food & Beverage Manufacturing Solutions

Electrical faults are only part of the picture.
Across the wider facility, fire risk can develop in places that are harder to monitor as traditional point sensors struggle to provide full-site visibility. Warehouses are filled with dense stock. Outdoor yards with constant vehicle movement. Waste and recycling areas where heat can build quietly. Traditional monitoring can be inconsistent, and false alarms from sunlight, steam, or machinery are common, increasing unnecessary disruption and callouts.
Thermal imaging takes a different approach. It continuously scans large areas, detecting abnormal heat and flame signatures as soon as they appear. In testing environments designed to replicate real conditions, thermal systems maintained over 94% detection accuracy with no false alarms, even under glare, headlights, and hot machinery.
This ensures fire risks do not go unnoticed between inspections or outside operating hours.
Thermal monitoring highlights overheating in breakers, busbars, and connections, allowing them to be identified early before failure. Early visibility enables teams to isolate issues quickly, reduce diagnostic time, and perform maintenance more safely without opening live panels.
Ovens, fryers, and packaging lines generate constant heat, which can mask developing issues. Continuous monitoring catches subtle changes against the baseline, helping prevent small issues from interrupting output by allowing teams to act before escalation.
High-density storage zones, loading bays, warehouses, and yard areas carry a higher risk of fire spread. Thermal imaging identifies hot spots early, helping protect inventory and infrastructure.
And in quieter parts of the site, plant rooms, chilled docks, and outbuildings, continuous monitoring fills the gaps left by limited staffing, keeping watch when no one is physically present.

When electrical monitoring and wide-area fire detection are combined, the result is a much clearer picture of risk across the entire facility.
Instead of isolated checks and reactive responses, teams have consistent visibility. They can prioritise work based on real conditions, respond more quickly when conditions change, and reduce exposure to both electrical faults and fire incidents.
That shift has a direct impact. Less unplanned downtime. Fewer disruptions to production. Lower risk to assets, but more importantly, people.
The early signs of fire and electrical failure are almost always there. The challenge is seeing them in time.
Thermal monitoring brings those signs into view, from small temperature changes inside a panel to heat patterns across an entire site. By identifying risks early, food and beverage operators can protect assets, maintain safe operations, and keep production running without interruption.
Explore how heat-related risks can be better managed across your facility