Such a problem commonly appears if the file structure of a LabVIEW program has been altered (e.g., moved to a new place). Try to search for the missing files manually in the locations below.
Parts of the Thermovision LabVIEW Toolkit are located in two places: the toolkit itself and examples. The root is the directory, containing LabVIEW. For example, if you use LabVIEW 2009 and it is installed as default, the toolkit can be found in:
C:\Program files\National Instruments\LabVIEW 2009\user.lib\ThermoVision\
and examples in:
C:\Program files\National Instruments\LabVIEW 2009\examples\ThermoVision\