FLIR Debuts Two High-Speed Thermal Cameras for Science and Research

Cameras Offer Faster Snap-shot Speeds and Higher Temperatures for Longwave Scientific Research

WILSONVILLE, Ore. – April 10, 2017 – FLIR Systems, Inc. (NASDAQ: FLIR) introduced today two high-speed, longwave thermal cameras for science and research applications, the FLIR X6900sc SLS and FLIR X8500sc SLS. Shown today at the SPIE Defense and Commercial Sensing convention in Anaheim, California, both cameras provide the faster frame rates, shorter snapshot speeds, and wider temperature ranges needed for the most demanding scientific research applications. 

The new thermal cameras are based on FLIR’s highest-speed, midwave thermal camera models, the X6900sc and X8500sc, but feature strained layer superlattice (SLS) detectors filtered for longwave infrared. These SLS detectors produce high frame rates and wide temperature ranges, as well as integration times that are more than 12 times faster than their midwave counterparts. FLIR combined this advanced technology with popular features of high-speed visible cameras, such as remote triggering and precise synchronization, to produce high-performance cameras that can capture meaningful data for anything from aerospace research to composite materials testing.

FLIR X6900sc SLS

This high-speed longwave thermal camera captures full-frame 640x512 thermal images at 1004 frames per second, at temperatures up to 3000 degrees Celsius. The FLIR DVIR™, a removable storage device that comes standard with the X6900sc SLS, saves up to 26 seconds of data to on-camera RAM without dropping frames. With advanced triggering options and an automatic, four-position filter wheel, this camera offers the functionality to stop motion on high-speed events both in the lab and at the test range.

FLIR X8500sc SLS

The X8500sc SLS records up to 181 frames per second of full 1280x1024 HD thermal imagery. This camera also features the FLIR DVIR which saves up to 36 seconds of data to on-camera RAM without dropping frames, and can measure temperatures up to 3000 degrees Celsius. The X8500sc SLS streams high-speed, 14-bit data simultaneously over Gigabit Ethernet, Camera Link, and CoaXpress for live viewing, analysis, or recording.

“Offering an SLS-version of FLIR’s X6900 and X8500 science cameras raises the bar on high-speed thermal imaging,” said Rickard Lindvall, Vice President and General Manager of FLIR’s Instruments segment. “The longwave SLS detector allows us to make a faster camera that can reach higher temperatures and yet still offer all of the cutting-edge functionality scientists and researchers have come to expect from FLIR.”

The FLIR X6900sc SLS and FLIR X8500sc SLS are available now for orders through established FLIR sales channels. For more information on these cameras, please visit www.flir.com/science.

About FLIR Systems, Inc.

Founded in 1978 and headquartered in Wilsonville, Oregon, FLIR Systems is a world-leading maker of sensor systems that enhance perception and heighten awareness, helping to save lives, improve productivity, and protect the environment. Through its nearly 3,500 employees, FLIR’s vision is to be “The World’s Sixth Sense” by leveraging thermal imaging and adjacent technologies to provide innovative, intelligent solutions for security and surveillance, environmental and condition monitoring, outdoor recreation, machine vision, navigation, and advanced threat detection. For more information, please visit www.flir.comand follow @flir.

Back to top