How long Composite Video cable can be used with the cameras?

No exact length can be given. The output amplifier is a video driver terminated by 75ohm. Depending on quality of cable and required quality of the video signal, more than 100m can work. On the other hand, if there is very high demands on the signal, for instance to make professional video recording, or if a low quality cable is used, 10m may be too much. Commercially available cable sets are ususally max 25m.

Back to top