Is it possible to get a full screen image including the menus from the camera video output to a monitor or video projector? Are there any other solutions to display the same image as on the camera LCD monitor?
It is not possible to get the wide image on the composite video output. Full screen display on a PC can be done via firewire and the small utility program FLIR IR Camera Player.
see download page for FLIR IR Camera Player 2.1.4