What is the highest object temperature the FLIR K series can see?

The second temperature range goes up to 650°C/1202°F. When the object temperature is above 650/1202°F°C the text >650°C or >1202°F will be displayed on the screen and any temperatures above 650°C/1202°F will have a dark red color. See the picture below.

Back to top