There may be a configuration change in the system made by another software installation that could be creating problems with FLIR Tools.
To identify the problem, send a query to FLIR customer support ( using Ask a question) with the following for us to analyze further and resolve the problem:
- The log directory zipped from the following location: "C:\ProgramData\FLIR Systems\FLIR Tools\Log" (this folder is hidden, so you need to copy the path within the quote marks and paste it into the Windows Explorer address bar).
- The "user.config" file present in the directory starting with "FLIR_Tools" from the location "%LOCALAPPDATA%/FLIR_Systems" (copy the path within the quote marks and paste it into the Windows Explorer address bar).
- From the Command prompt, execute the following:
(a) PATH > PATH.TXT
(b) notepad PATH.TXT
Save the "PATH.TXT" file that will be created onto your Desktop, and send it to us together with the previous two files.