Register for our Category I Course
October 22-25, 2024 - Auckland (Takapuna Boating Club)
The Cat 1 Infrared Thermography Training Course is geared to the new infrared camera user and focuses on its use for a variety of condition monitoring/predictive maintenance applications. Attendees completing all training course requirements and a thermography field assignment will receive a Cat 1 Infrared Thermography Certification.
Course Description
Benefit
- Introduction to thermal imaging and measurement systems for predictive maintenance applications.
- No experience in thermography is necessary!
- Collect quality data, accurate temperature readings, and account for measurement effects such as distance and emissivity using infrared cameras.
- Interpret thermograms and make informed decisions using heat transfer concepts to analyze thermal images, and see the latest in infrared inspection report generation and database software.
- Avoid costly mistakes - learn to distinguish between hot spots and reflections, direct vs. indirect readings and qualitative vs. quantitative thermography.
- Challenge yourself with field applications labs that closely simulate real-world infrared applications.
Recognition
All ITC thermographers are certified against one or more of the following standards:
- EN473 recommendations for qualification and certification of non-destructive testing (NDT) personnel, as established by the European Federation and accepted by the American Society of Mechanical Engineers (ASME);
- ISO 9712 specifying proficiency in infrared thermographic testing as related to the qualification and certification of personnel involved in non-destructive testing (NDT), as established by the International Organization of Standardization (ISO) TC 135/SC 7;
- ISO 18436-8: Requirements for thermography training and certification of thermography personnel in condition monitoring and the diagnostics of machines, as established by the International Organization for Standardization (ISO) TC 108/SC 5.
Your Presenter
Dr Ken Jackson has a PhD from the University of New South Wales in Sydney, Australia. His research there included extensive use of Infrared microscopy in the study of catalytic pathways. Dr Jackson has used and trained in Infrared and other analytical techniques for more than 20 years. Dr Jackson is an Certified Level III Thermographer and has been running training courses in Infrared Thermography in New Zealand and Internationally since 1998.
Cost
$2,700 NZD/person + GST, which includes examination and certification.
Your place will be reserved and guaranteed upon receipt of payment.
Duration: Four consecutive days.
If you need more information about the course, please contact steven.blott@teledyne.com.