How a Heavy-Duty Thermal Camera Stand Accelerates Testing and Research for Close-up Electronics Work

Quick, Stable Support for Infrared Microscopy and Close-up Lens Systems

If you’ve ever tried to capture high‑magnification thermal data on integrated circuits or other small components, you know the frustration. Every micro‑adjustment costs time, and the higher the magnification, the more unforgiving small changes and vibrations become.

Mounting a heavy, high‑magnification infrared camera over a tiny and often expensive test target is precarious, challenging, and slow. Even once you secure it, small vibrations from cooling systems or bench movement can cause the focus to gradually shift, forcing repeated adjustments. The higher the magnification, the more punishing even small vibrations become.

Engineers end up chasing hot spots across blurry images. Researchers spend too much time trying to align visual and thermal views for publishable work. And when your system is cobbled together with generic microscope stands or boom arms, even slight movement can ruin a test; or worse, a valuable camera could be dropped.

You’re left fighting the setup instead of analyzing the data.

“Historically, there really hasn’t been any good, off‑the‑shelf solution for mounting heavier, high performance cooled thermal cameras vertically over test articles. People would typically use a microscope boom arm or cobble something together using whatever they had lying around. This approach typically produced camera mounting systems with insufficient mechanical stability for reliable, high-quality thermal measurements,” said Jerry Beeney, Director of Sales - Americas Science & Global BD, Flir.

A Camera Stand Engineered for Stable Support

The Flir Heavy Duty Open Base Camera Stand combines precision, stability, and flexibility in a single system. Developed based on direct customer feedback, the camera stand offers both quick and very fine Z-axis control so you can lock focus at high magnification without focus drift.

Its heavy-duty structure minimizes vibrations, allowing you to maintain clear, stable thermal imagery during sensitive inspections. Its open base design provides a generous workspace beneath the camera, whether you’re testing large assemblies, attaching probes, or introducing environmental variables. And because the stand is built from industry standard 80/20 components, you can add stages, brackets, or customized fixtures without a custom machining project.

The microscope-style stand also supports all Flir research & science cameras—from A50 through the X Series—so it stays relevant as your imaging needs scale, whether you’re working with uncooled microbolometers or high sensitivity cooled infrared systems.

Flir X-Series camera on the heavy duty base

Designed for Precision in Thermal Testing

Flir engineers designed the Heavy Duty Open Base Camera Stand around three customer‑driven requirements:

1. Improved Stability: Reduce vibrations and enhance image quality

High end thermal cameras are inherently heavy, with internal coolers and large precision optics that make them particularly sensitive to vibration. When operating at small spatial resolutions, especially with high-magnification optics, even minor mechanical movement can introduce image blur and compromise measurement accuracy.

Generic stands are typically unable to provide the rigidity and damping required for these conditions. The Flir stand addresses this challenge with a heavy-duty frame engineered specifically to support the camera mass and minimize vibrational movement, ensuring the stability required for high-resolution thermal imaging and repeatable, reliable results.

2. Precision Focusing: Quick and extremely fine Z‑axis control

Testing often requires frequent refocusing, especially when switching between standard, macro and microscope objective lenses. The stand’s dual‑mode Z‑axis control allows users to reposition quickly, then refine precisely.

“With high‑magnification lenses, even tiny vibrations show up in your data. That’s why we built in a heavy‑duty structure and fine Z‑axis control, so you can focus once and start measuring,” said Michael Roselli, NE Sales Engineer, Research & Science Cameras

3. Simplified Setup: A safer, easier mounting process

Mounting a cooled thermal camera to a vertical stand typically requires holding the heavy camera with one hand while installing and tightening fasteners with the other, a nerve‑wracking process when trying not to drop an expensive piece of sensitive equipment.

“With previous stand designs, users had to physically support a heavy, high‑value camera in a vertical position while trying to line up the mounting screws with the base plate, which was both awkward and risky,” said Beeney. “This new camera stand was designed to remove that burden entirely. It allows the user to place the camera into the correct orientation first and then securely fasten it with a simple, one‑handed motion.”

The result is a safer, more efficient setup process that significantly reduces handling risk and improves overall usability. This greatly reduces the risk of drops, slips, or damage to highly valuable prototypes.

Engineers: Find Hot Spots Faster, With Confidence

For engineers validating designs or trying to isolate points of failure, time and clarity matter. A stand that lets you keep the camera stable and precisely aligned means you:

  • Identify hot spots faster
  • Acquire crisp thermal images
  • Can quickly correlate good and bad test articles
  • Avoid the need to retest components due to poor focus
  • Keep cameras and other equipment safe during frequent re-mounting

“Engineers working with a wide range of test articles especially benefit,” says Roselli. “Whether they’re imaging small PCBs or larger assemblies at different heights, the stand easily adapts while maintaining consistent optical alignment – meaning the setup doesn’t have to be reworked every time the test configuration changes.”

When paired with Flir’s broad portfolio of research & science cameras and lens options, from A Series through X Series, the stand gives engineers full imaging flexibility, from wide, full board views to tight macro focus for achieving extreme detail when inspecting small, densely packed components.

Researchers: Precisely Align Visual and Thermal Data

Research teams don’t just need thermal images that look good, they need accurate temperature information they can rely on to make critical decisions, defend in peer-reviewed papers, or share with collaborators.

The stand’s stability is essential to maximizing the power of merging infrared data with visible imagery through the Flir Static MIX feature included in the Flir Research Studio  professional edition software, giving engineers and researchers the ability to:

  • Correlate temperatures with physical structure
  • Improve their understanding of complex interactions
  • Reduce post‑processing times
  • Eliminate errors due to lack of visual context

However, these capabilities depend on clear, repeatable thermal imagery – something that improvised stand solutions cannot reliably guarantee.

With the Flir heavy-duty camera stand, researchers can acquire crisp thermal imagery, generate informative infrared and visible overlays, provide clearer documentation, and benefit from reproducible setups. And for situations where cameras need to be removed and stored between uses, the ability to re‑mount the camera without disturbing the position of the stand is especially valuable.

The Flir Camera Stand Does What Others Can’t

Most generic microscope stands fail for at least one of these aspects:

  • Not rated to support heavier cooled thermal cameras
  • Cannot dampen vibration from internal coolers
  • Not stable enough for high‑magnification optics
  • Lack precise Z‑axis control
  • Require ad-hoc adapters to fit IR cameras
  • Make mounting precarious or awkward
  • Have limited workspace under the camera

Flir’s stand solves all of these at once.

BUY THE STAND

Packages Offer Greater Value and Faster Setup

The stand itself delivers meaningful value, but its full benefit is realized when purchased as part of one of Flir’s purpose-built A6701 research packages.

Each package includes:

  • A Flir A6701 mid-wave infrared camera
  • The heavy‑duty open-base stand
  • Flir Research Studio Professional Edition software
    • Choice of either a 17 mm, MWIR Macro lens, or 1X microscope objective lens

These packages eliminate the problem of ad-hoc, cobbled-together cameraT stands entirely. With a single order, users receive a fully integrated system with everything included, engineered to work together, and offered with special pricing.

In the end, the FLIR Heavy Duty Open Base Camera Stand succeeds where generic stands fall short. Most off-the-shelf options are not designed to support the weight of cooled infrared cameras, nor can they provide the mechanical stability and repeatability required for high-resolution, closeup thermal measurements.

The Flir Heavy Duty Open Base Camera Stand lets your camera—and your data—perform at their highest potential.

Learn more about Flir’s purpose built A6701 research packages. 

 

Back to top