Reducing Hidden Risks in Food & Beverage Production


From processing to packaging and storage, every step in the manufacturing of food and beverages has potential risks. Even a small temperature change or an invisible packaging flaw can lead to wasted products, safety issues, or product recalls. These hidden risks make it hard for manufacturers to maintain high-quality standards.
With the global food safety market projected to reach $31.1 billion by 2027, demand for stringent food and beverage safety measures is growing rapidly.
Despite their widespread use, spot checks and visual inspections were never designed to provide continuous oversight. They offer confirmation at a specific point in time, not across an entire production run or storage cycle. In fast-moving manufacturing environments, that limitation creates exposure.
To truly manage risk, manufacturers need visibility across the full production environment, from cooking and processing to packaging, storage and distribution; continuous monitoring ensures no stage is left unchecked. Subtle temperature variations, micro-leaks in packaging, or faulty refrigeration are detected in real time. This holistic approach transforms safety and quality from reactive fixes into proactive control, protecting products, personnel, and profits simultaneously.

Below are some of the key reasons why spot checks alone are no longer sufficient in modern food and beverage production.
Small temperature inconsistencies in food preparation or processing may not be visible or measurable through periodic probe checks. Surface temperature variations indicating undercooking, overheating, or irregular product distribution often go undetected without continuous, real-time monitoring. With 6001 million people globally becoming ill after eating contaminated food every year, and 25%2 of contamination incidents being directly caused by pathogenic micro-organisms in food products, undetected temperature changes are a big issue for the food and beverage industry.
See all of our Food & Beverage Manufacturing Solutions
Many manufacturing procedures require manual checks or periodic inspections, leaving gaps between control points. Small deviations can go undetected for hours or even days. Hidden risks, such as uneven cooking temperatures or heat buildup in machinery, can often go unnoticed until it's too late, resulting in entire batches being affected before anyone spots the issue. By integrating end-to-end thermal monitoring across every stage, manufacturers can close these gaps, ensuring consistent quality.
The average direct cost of a food recall is around $10 million per incident. Adhesive gaps, inconsistent glue bead thickness, or weak seals may pass visual inspection. However, these small defects can later lead to contamination, leakage, and recalls. Spot checks simply can’t verify every seal across every product at production speed. Continuous thermal inspection across the entire packaging line provides full visibility into seal integrity and fill accuracy, catching defects that would otherwise go unnoticed until after distribution.
When a fire is not caught early, it can cause serious financial, environmental, and commercial distress for a company and the community, and even “contained” incidents can still cause costly damage, downtime, and product loss. Conventional fire sensors often respond once smoke or flame reaches them. This delay limits coverage and slows response time. By the time a spot check or traditional alarm is triggered, the production line would need to be stopped.
Approximately one-third of all food produced worldwide is lost or wasted along the supply chain. Preventing spoilage at crucial refrigeration points helps to reduce the volume of product discarded due to temperature excursions, equipment failure, or undetected performance drift. With refrigeration systems rarely failing at once but gradually falling out of specification, detecting refrigeration issues is difficult. When monitoring is extended across the full storage environment, small deviations in refrigeration can be flagged immediately, preventing product loss and protecting both margins and sustainability goals.
Compressed air can account for a significant portion of industrial energy consumption, yet leaks frequently go undetected. Many are impossible to hear in noisy utility rooms. As leaks grow, compressors cycle harder, energy bills rise, and system reliability declines. Spot checks cannot reliably detect invisible or inaudible losses.
Hidden risks in food and beverage production don’t have to disrupt operations. With continuous thermal monitoring, manufacturers gain full visibility across every stage of the line, ensuring safety, quality, and efficiency. By proactively identifying and addressing issues, teams can maintain uptime, reduce waste, and protect both products and personnel.
Key benefits of thermal monitoring in food and beverage production include:
Flir offers a range of thermal cameras designed specifically for food and beverage production, providing tailored solutions at every stage of the process. From smart sensors to advanced imaging systems and wide-range modes, there is a solution for every control point.
Explore today to see how thermal imaging can transform your production line.
1 www.who.int/news-room/fact-sheets/detail/food-safety
2 www.food.gov.uk/board-papers/incidents-resilience-unit-annual-report-202324