Flir One Edge Is Now Flir Edge: Same Trusted Innovation, Simplified Name

At Flir, we’re always looking for ways to make it easier for customers to find, understand, and use our technology. That’s why we’re simplifying the name of our award-winning mobile thermal camera series: Flir One Edge and Flir One Edge Pro are now Flir Edge and Flir Edge Pro.

This change reflects how the series has evolved beyond the original Flir One family to become a next-generation solution for professionals who need powerful, wireless thermal imaging in the field.

Product Line Update

Here’s how the new and existing models align:

Product Previous Name Native Resolution With Super Resolution
Flir Edge Pro Flir One Edge Pro 160 × 120 480 × 360
Flir Edge Flir One Edge 80 × 60 240 × 180
Flir One Pro

(Unchanged)

160 × 120 480 × 360
Flir One Flir One Gen 3 80 × 60 240 × 180


Going forward, FLIR ONE Gen 3 will simply be called Flir One.

Why the change?

The updated naming makes it easier to navigate our mobile thermal imaging portfolio.

  • “Flir Edge” now stands on its own as the newest generation in the lineup, designed for flexibility, connectivity, and professional use.
  • “Flir One” remains the trusted compact thermal camera series.

Flir Edge and Flir One Series: Thermal vision that fits in your pocket

  • Enhanced smart phone connectivity – seamless iOS® and Android™ pairing
  • Flir Edge Pro and Flir One Pro feature VividIR™ with Super Resolution 480 x360 (Native IR 160 x 120)
  • Flir Edge and Flir One feature VividIR™ with Super Resolution 240 x 180 (Native IR 80 x 60)
  • Compact and durable clip-on design, IP54-rated, drop tested

What happens next?

If you’ve previously searched for or owned a Flir One Edge, don’t worry—all product pages and resources will automatically redirect to the new Flir Edge pages. You’ll continue to receive the same product support, firmware updates, and accessories.

Looking ahead

The Flir Edge series represents the next chapter in mobile thermal imaging—a bridge between the simplicity of Flir One and the power of Flir’s professional cameras. We’re excited to keep innovating to help you see the unseen, capture critical data, and make better decisions faster.

 

관련 기사

사례 연구

FLIR ONE® Edge Pro를 활용해 자동차 검사를 간소화하는 5가지 방법

Read more
기사

Top 5 Ways to Use FLIR ONE on Your Smartphone

Read more
Back to top