Featured Integration: iXX + ExView

Connected Measurements: Extech ExView® App Now on Flir iXX Cameras

A key new addition to the ACE ecosystem is the Extech ExView® app, bringing connected measurement capabilities directly to iXX cameras and enabling inspectors to collect, visualize, and document meter data.

 

Why Connected Measurements Matter

Whether evaluating electrical equipment, mechanical systems, building conditions, or indoor environmental quality, technicians frequently need measurement data to support thermal findings.

Questions such as:

  • What was the ambient temperature during the inspection?
  • How did humidity affect the area being evaluated?
  • Are airflow conditions contributing to the problem?
  • What supporting measurements validate the thermal anomaly?

Traditionally, collecting this information required manually transferring readings into reports. The ExView app helps eliminate this gap by enabling wireless Extech devices to communicate directly with the ACE platform.

A Better Field Experience

With ExView running directly on the camera, inspectors no longer need to switch between a thermal camera and a separate smartphone or tablet. All inspection information can be managed from a single device.

 

From Measurements to Actionable Reports

Data is most valuable when it can be communicated clearly.

The ExView platform was originally developed to simplify data collection, visualization, and reporting from connected Extech meters. On the iXX platform, that same philosophy helps users move efficiently from inspection to documentation.

Inspectors can capture measurement information during the inspection process and incorporate supporting evidence into their workflow, reducing the time spent manually compiling reports after returning from the field.

The result is a more complete picture of asset condition and a more professional deliverable for customers, maintenance teams, and decision makers.

Expanding the ACE Ecosystem

The ExView app demonstrates the flexibility of the ACE platform and the growing vision behind the iXX Series. The ACE ecosystem enables first-party and third-party applications to extend the value of thermal cameras beyond image capture. By integrating connected measurement tools, Cloud services, reporting solutions, and workflow applications, iXX helps customers solve real-world inspection challenges more efficiently.

 

Get Started

The ExView app is completely free and can be installed from Flir Apps+. See below list of compatible products:

Back to top