Flir Scout Pro Supports Officer Safety at Pelham Police Department

Located in southern New Hampshire near the Massachusetts border, the town of Pelham presents unique challenges for its police department. With dense woodlands, power line corridors, and a mix of residential and commercial areas, officers often find themselves searching large areas in low-light conditions where traditional visibility tools fall short.

For Corporal Cody Halliday of the Pelham Police Department, thermal imaging has become an essential tool for improving officer safety and situational awareness in the field.

Drawing on 11 years of experience in the National Guard—where he extensively used thermal systems, primarily larger mounted platforms—Halliday brings a unique perspective to law enforcement applications of thermal technology. Today, he also helps train fellow officers on the many ways thermal imaging can be used during police operations.

“When using thermal imaging, there are a ton of applications, and we often get tunnel vision on what thermal capabilities can do,” said Halliday. “They can do a lot, day or night. You just need to know how to apply it, use it, and understand best practices.”

Portability and Palette Options

The Flir Scout Pro’s compact design addresses a critical need for law enforcement officers who already carry a wide range of equipment.

“Keeping it about the size of a cargo pocket is ideal,” Halliday explained. “Especially for law enforcement—we have so many tools on us, and we have limited space to carry things. I want to be able to grab that from a cruiser bag and throw it in my cargo pocket.”

This portability proved valuable during a recent investigation when a suspect fled into dense woods.

"It was a burglary suspect who ran into a treeline after we had set a perimeter," Halliday recalls. "Just having that camera with us, especially in a high-stakes call like that. Often, burglary suspects are armed. It gets very dangerous when we start going into the woods and we can't see what's going on."

Thermal imaging allows officers to scan large areas quickly and identify heat signatures without relying on visible light.

Superior Performance, Simplified Operation

The Flir Scout Pro thermal imaging camera revealing a person hiding under the staircase

Halliday also highlighted how the Scout Pro simplifies operation in demanding environments.

Law enforcement demand simplicity above all else. 

“The Scout Pro auto-adjusts quickly with no lag, which is super helpful because it takes that guesswork out of it. I need to be able to use it in the dark without looking at the buttons, and I need to be able to do it just for safety." 

The Scout Pro’s 32-degree field of view, which is wider than many competing thermal imaging monoculars, also stood out.

“That wider field of view compared to other units means it doesn’t feel like you’re looking through a tunnel,” Halliday noted.

A wider view allows officers to scan areas more efficiently, improving awareness when moving through wooded terrain or large outdoor spaces.

Night Patrols

Beyond search operations, the Scout Pro has become part of Halliday’s routine patrol work.

"Even when I'm on patrol, I'll check a parking lot real quick. Let's say it’s two in the morning, I would look to see if a car is running that shouldn't be there because we’ve had catalytic converter thefts, people stealing parts, or staging for some other crime."

When Halliday spots a running vehicle in a closed parking lot during the early morning hours, it immediately raises red flags. 

"That stands out. That's odd. Why is that car running in this parking lot at two in the morning? It's been closed for six plus hours. They shouldn't be there. So now I can go touch base and I know someone's there without getting surprised."

Thermal imaging helps officers quickly detect activity without alerting suspects or relying on bright lights that could reveal their position.

Distraction-Free K9 Operations

Halliday and other officers often work with canine units from neighbouring agencies during searches for suspects or missing persons. In these situations, thermal imaging provides a critical advantage.

Using thermal imaging eliminates the need for flashlights that could interfere with the search.

"During searches with K9s, you don't want to backlight the officer or the dog because it's unsafe. Suspects then know your location, but more importantly, it's distracting for the dogs," Halliday explained. "Having a Flir is spectacular because instead of having to use a flashlight or walking around in the dark in the woods, you can use a thermal and scan. You're giving no light signature, and it doesn't affect the dog."

A Practical Tool for Modern Policing

Flir Scout Pro™

Der Flir Scout Pro ist das thermische Monokular der nächsten Generation, das für und mit Fachleuten für Strafverfolgung und öffentliche Sicherheit entwickelt wurde. Der Scout Pro wurde für den zuverlässigen Einsatz bei Missionen mit hohem Risiko entwickelt, bei denen Zeit und Konzentration entscheidend sind. Er bietet vereinfachte Bedienelemente, damit Sie sich nicht in den Menüs verirren, robuste Haltbarkeit, um rauen Bedingungen standzuhalten, und Live-View-Funktionen, um Ihr Team in Echtzeit zu informieren. Mit einem Objektiv mit festem Fokus und einem 32°-Sichtfeld – dem breitesten auf dem Markt – ermöglicht der Scout Pro schnelle Flächenbewegungen und identifiziert menschliche Wärmesignaturen bis zu 500 Meter entfernt, selbst bei Dunkelheit. Die fortschrittlichen Bildverbesserungen sind speziell auf die Erkennung von Menschen zugeschnitten, so dass Sie nie ein Ziel verfehlen.

For departments like Pelham, thermal imaging is quickly becoming a critical capability for modern policing.

Compact, intuitive, and designed for field use, the Flir Scout Pro helps officers detect threats earlier, search more effectively, and operate more safely during night patrols and high-risk calls.

As Halliday’s experience shows, thermal imaging is no longer just a specialised tool—it’s becoming an essential part of everyday law enforcement operations.

 

Info anfordern

Optin

Mit der Übermittlung stimmen Sie der Datenschutzrichtlinie und Cookie -Richtlinie von FLIR zu.

Back to top