FLIR Launches High-Performance Thermal Camera for Long Range and Science Applications

New FLIR RS8500 Combines a Mid-Wave Thermal Detector and Telescope to Acquire Data on Long-Range and High-Temperature Targets in Harsh Environments

ARLINGTON, Va., May 7, 2020 – FLIR Systems, Inc. (NASDAQ: FLIR) today announced the FLIR RS8500 mid-wave infrared (MWIR) thermal camera designed for range tracking, science, and measurement applications. A new addition to FLIR Systems’ science camera series, the high-performance RS8500 combines a mid-wave infrared detector and telescope in a single weatherproof housing built for measurement accuracy of long-range and high-temperature targets in harsh environments.

The RS8500 allows for superior measurement accuracy through a MWIR detector, which provides high-definition, large-format thermal images with the ability to deliver data up to 180 frames per second, coupled with a high-resolution, 120-1200-millimeter continuous metric zoom lens. This provides maximum situational awareness at wider fields of view and zoom capabilities at longer focal lengths to maximize the number of pixels on a target at any distance. The camera also has the capability to image through neutral density filters, ensuring that hot targets do not look saturated. Further, the RS8500 offers 24 percent more pixels and a 46 percent faster frame speed than the previous RS8000 models. 

RS8500-Appl-FL-01-0420.jpg

“With higher resolution and simplified data analysis, the FLIR RS8500 is an optimal thermal camera solution for applications in industries such as outdoor research, military, aerospace, university and government labs, and film production,” said Rickard Lindvall, General Manager of the Solutions Line of Business at FLIR. “This new mid-wave camera provides the ability to accurately measure high- temperature, fast-moving targets at a greater distance and ensure operator safety.”     

The RS8500 also provides one graphical user interface and multiple simultaneous data outputs which allows for easy integration of the camera into existing data acquisition systems as well as FLIR Research Studio. 

The FLIR RS8500 is available globally for purchase today. For further information please visit www.flir.com/RS8500.   

Zugehörige Artikel

Neuigkeiten zu Produkten

FLIR Introduces Next Generation of Compact, High-Definition Thermal Science Cameras

Read more
Neuigkeiten zu Produkten

New High-Performance Infrared Cameras for Science and Research

Read more
Neuigkeiten zu Produkten

Two New Longwave, High-Speed Thermal Cameras

Read more
Back to top