From Zero Guesswork to Zero Outages: How Flir and Hi-Tech Enabled NALCO’s Smart Substation Transformation


Reliability is everything in high-demand industrial environments, and nowhere is this more critical than in an aluminum smelter.
At NALCO’s Angul plant, the engineering team set out with a clear and ambitious objective: eliminate unplanned outages by achieving continuous visibility across their 220kV switchyard. In this environment, even a momentary power disruption can halt production, damage equipment, and result in significant financial loss.
What was needed was not simply faster inspections, but a fundamental shift in how assets were monitored. The team required a way to move beyond periodic checks toward continuous, predictive insight—a solution that could detect issues early, reduce reliance on manual intervention, and improve safety by minimizing exposure to high-voltage areas.
By deploying always-on thermal imaging and intelligent analytics, Flir helped convert NALCO’s switchyard into a data-driven “Smart Yard” where critical assets are monitored in real-time and risks are identified before they escalate.
With Flir’s solution in place, NALCO achieved:
The shift to automated condition monitoring allowed the team to move away from reactive maintenance toward predictive, insight-driven operations delivering both operational reliability and long-term cost savings.
![]() |
![]() |
Before implementing Flir technology, maintenance relied on manual, periodic thermal inspections. While useful, these inspections provided only snapshots of an asset’s condition, leaving extended periods where faults could develop unnoticed. Issues could emerge immediately after an inspection and remain undetected until the next cycle, increasing the risk of unexpected failure.
Manual inspections also introduced safety concerns. Engineers were required to assess high-voltage components directly, exposing them to hazardous conditions and operational risk.
Environmental factors made detection even more difficult. High humidity and harsh operating conditions contributed to corrosion and thermal anomalies that were often invisible during routine checks.
Together, these limitations meant that even well-managed inspection regimes could not deliver the level of certainty required. Without continuous monitoring, early warning was simply not possible.
To address NALCO’s maintenance challenges, Flir worked with partner Hi-Tech to implement a Continuous Condition Monitoring System tailored to their operational needs— one that was designed to provide full visibility across critical electrical infrastructure.
The solution integrates Flir Axxx fixed thermal cameras, automated pan-tilt units, and advanced monitoring software into a unified system. Transformers, circuit breakers, and key connection points throughout the switchyard could now be continuously monitored thanks to the new system.
|
Flir Axxx-Series Camera |
PT Housing |
Installation Site |
Flir’s approach goes beyond imaging, it focuses on delivering actionable insight.
High-resolution thermal cameras detect even minor temperature variations, enabling early identification of potential failures.
Pan-tilt units automate inspection routines, ensuring consistent and repeatable monitoring without reliance on manual processes. At the same time, Flir’s intelligent software maps each asset and continuously tracks condition data.
When temperature thresholds are exceeded, the system immediately identifies the affected component and triggers alerts. Maintenance teams receive real-time notifications, allowing them to respond quickly and prevent escalation.
The combination of continuous sensing, automation, and analytics enables operators to transition from inspection-based workflows to predictive condition monitoring.

The real value of transitioning to continuous, automated monitoring lies in how it changes day-to-day operations.
For the NALCO team, what was once a manual and reactive process is now automated and insight-driven. With continuous monitoring and instant alerts, engineers can identify issues earlier, prioritize maintenance activities, and reduce the likelihood of unexpected failures.
At the same time, the need for personnel to operate in high-risk environments has been significantly reduced, supporting safer working conditions.
The result is a more efficient, proactive approach to asset management, one that improves both reliability and safety while supporting uninterrupted production.
By enabling continuous thermal monitoring, Flir has helped NALCO redefine how critical infrastructure is managed.
Instead of relying on periodic inspections and reactive responses, the switchyard now operates as a predictive, data-driven system, where potential risks are identified early and addressed before they impact operations.
This transformation demonstrates how thermal imaging can go beyond inspection—delivering actionable intelligence, improving safety, and driving measurable business outcomes.
At Flir, the goal is simple:
Work with partners like Hi-Tech to help industrial operators move from uncertainty to control—turning zero guesswork into zero outages.