The FLIR - Software House module integrates CCure 9000 with the FLIR United VMS (Latitude, Horizon and Meridian), allowing CCure to act as the front end. The integration expands CCure 9000 capabilities by allowing users to view live and recorded video from FLIR United VMS cameras within the CCure 9000 user interface. Users can also monitor events, control PTZ cameras, trigger actions, display OSD, export video and more, right from the comfort of their CCure 9000 monitoring station.
Key Features
Display live view of a single or group of cameras manually or upon an event
Display recorded video right from the C•CURE 9000 Activity Viewer
Configure access control actions upon video and analytics events
Control PTZ cameras right from the CCure monitoring station
Export video with the flexibility of choosing length, file size and video format
Save and email a snapshot of either live or recorded video
Connect to multiple FLIR United VMS servers from within the same application
Video Monitoring
Display a live view of a single or group of cameras manually or upon an event
Integration supports import or manual creation of VMS-controlled cameras
Users can easily identify the camera being viewed by an enhanced on-screen display of the camera name, date/time and live recording or playback status
Integration supports C•CURE 9000 maps — users can add FLIR controlled cameras to the C•CURE 9000 maps and monitor the state of the cameras and pop up a live view of a camera directly from the map
The module provides seamless integration with C•CURE 9000 PTZ and on-screen PTZ controls
Users can monitor video events such as motion detection, relay and analytics, for instance, Intrusion Started / Ended, Vehicle Stopped, Unattended Object and Object Removed
Recording and Playback
Users can display recorded video directly from the C•CURE 9000 Activity Viewer
Query for recorded clips of a specific camera, according to start and end date / time is supported
Users can control playback of recorded clips
Events, Triggers, and Actions
Users can configure access control actions upon video and analytics events which allows the user to query for events by the person’s name later
Users can configure video actions upon access control events, such as start recording
System
Integration supports video export with flexibility to choose length, file size and video format
Users can save and e-mail a snapshot of live or recorded video
Multi-directory support allows a C•CURE 9000 operator to login to different systems from within the same application
Directory failover is supported
United VMS Infrastructure
Users enjoy the range of VMS features including: support of the most popular IP camera brands and encoders, use of multiple video compressions, resilient architecture that supports camera, encoder and server failover and more.
The highly customizable VMS Control Center client application can provide additional flexibility in viewing, recording and exporting audio and video to satisfy the needs from more.
Completes complex video and audio tasks, as well as monitoring a wide range of events and alarms. The advanced features of FLIR’s United VMS are always available for its users.
About Software House
Software House has built a solid reputation in the security industry as an innovator of security and event management technologies. With its continuous investment in R&D and the ability to leverage new technologies, Software House has worked hard to reach technological excellence. Reliability, flexibility and power are why many companies choose Software House solutions for their security needs. By holding true to those three qualities, Software House technologies have become the solution of choice for thousands of security-conscious businesses around the world. These solutions are put to the test every day at nearly 10,000 sites worldwide. They are designed to be a part of your business infrastructure and have been engineered to grow as your business grows. There’s no other security solution on the market that gives you the extraordinary level of control that Software House solutions provide. Software House solutions put you firmly in control of streamlined business operations.