It is possible to set up the camera network settings using a Telnet client program (Windows has native support for Telnet client, but it is not enabled by standard).
The commands to set the IP address of the FLIR A310 camera through a Telnet connection are:
Access to network resources:
rcd services.net.interface.LAN90001
Change the parameters (use quotation marks):
rset address "ip-address"
rset netmask "subnet-mask"
rset gateway "gateway"
Verify information entered:
rls
Confirm changes:
rset commit true