Object parameters in the FLIR K series are set to the following and are not possible to change.
- Emissivity: 0.95
- Atmospheric temperature: +60°C (+140.0°F)
- Relative humidity: 75%
- Distance to object: 3.0 m (9.8 ft.)
Object parameters are used in the formula to calculate the object temperature.