Is it possible to combine multiple FLIR Word reports into one document?

Yes, this is possible. To do this, follow the steps below:

  1. Create individual Word reports as usual. These are the parts to be combined.
  2. Open one of the Word reports.
  3. Go to the end of the report and click on the cursor below the last item in the report.
  4. Go to the Insert menu and click on page break.
  5. A new page wil be created.
  6. Go to Object and click on the dropdown list next to the object in the same Insert menu.
  7. Click on Text from file and select another Word report that you created in step 1.
  8. The two Word reports will now be combined.
  9. Click Save as PDF from the Word report to create a PDF report if you require a PDF file.
Back to top