Is there an event or status value that can be use in the code to see when it is time to do NUC?

There is no event or flag to see that it is time to do NUC. The red warning is generated by the camera control as below:

  1. NUC by time. 15 minutes or less should be OK.
  2. NUC at shutter temperature change >0.5°C. Read temperature by Properties 63 and 64. Resource for A40 is “.system.tempsens.shutter”
    If you use A320, A325 or SC6xx, the resource is different, please refer to command manuals.
Back to top