The following parameters will be reset when restoring factory default settings:
- Temperature unit is reset to: °C.
- Thermal indication is reset to: Reference bar.
- Date format is reset to: YY/MM/DD (the date is not changed).
- Time format is reset to: 12H (time is not changed).
- Number of active modes is reset to 5.
- The custom logo is deleted.