Why do I get a lower frame rate when recording in ResearchIR with my Ethernet camera than that specified for my camera?

Ethernet cameras, especially high-speed cameras, require a high bandwidth, and the bottleneck that could be the cause for not obtaining the specified frame rate may due to the network card on your computer.

If you have a Fast Ethernet network card, your network card will be capable of 100 Mbit/s, whereas if you have a Gigabit Ethernet network card, you will be able to acheive 1000 Mbit/s (1 Gbit/s).

Some cameras requires more that 100 Mbit/s, and if you have only Fast Ethernet you will not be able to obtain the specified frame rate. 

A good rule of thumb to calculate bandwidth requirements is as follows:

  1. Multiply the pixel width and pixel height of the image. 
  2. Multiply the result by the frame rate (Hz)
  3. Multiply the result by 16, since each pixel consists of 16 bits (even if the camera has a lower dynamic range such as 13 or 14 bit) 
  4. Divide by1 000 000 to obtain the required bandwidth in Mbit/s.
Back to top