Why do I get a Save As dialog when the wizard is generating a template preview?

For the template preview to work properly in the wizard, you need to install a printer.

If you don't have a printer, we recommend that you install one of the default printers that comes with Windows.

To install a default printer

  1. In the Windows Start menu, select Printers and Faxes.
  2. Under Printer Tasks, click Add a printer to open the Add Printer Wizard, and then click Next.
  3. Click  Local printer attached to this computer, and then click next.
  4. Windows will now search for a Plug and Play printer installed. If Windows fails to find a Plug and Play printer click next.
  5. Use the Recommended Printer Port, and then click next.
  6. Choose any of the printers in the list, and then click next.
  7. Select Yes when prompted if you want to use this printer as the default printer, and then click next.
  8. Select No when prompted to print a test page, and then click next.
  9. Click Finish to install the printer.

 

Back to top