I like to add several areas to measure the temperature. How many areas can I define using the camera built-in software?

The cameras with built analysis can have this many areas and spots:

Camera  Areas  Spots
A20, A40, A320  4  4
A310  10  10
AX8  6  6

A20, A40 and AX8 are set up using buttons on the camera or the Web interface. To set up the A320 or A310, use the IR Monitor utility.

Back to top