Using the Create panorama image feature does not combine all images together. Why is that?

The Create panorama image will usually work best if the images are taken at the same distance, with same focus and same zoom factor.

In order to create a panorama image a minimum of 30% overlap is required between consecutive images. Preferably, the images should be taken standing at the same position.

Back to top