Improving Food & Beverage Safety with Real-Time Thermal Imaging


Every year, around 600 million people fall ill after eating contaminated food, according to the World Health Organization (WHO). Behind these numbers are real families, hospital visits, and, in the most severe cases, loss of life.
In food manufacturing, a few degrees can make the difference between safe products and a costly recall. For manufacturers, even minor temperature deviations can trigger rejected batches, failed audits, unplanned downtime and damage to brand reputation.
The challenge is not knowing that temperature matters. It is monitoring it continuously without slowing production. That is where real-time thermal imaging delivers measurable operational value.
Cooking, pasteurisation and cooling are critical control points in any HACCP plan. Consistent heat is one of the most effective ways to prevent microbial contamination, but high-speed production lines make uniformity difficult, and slight temperature variations can quickly turn into larger problems if they aren't caught early.
Manual spot checks leave gaps. Between inspections, temperatures can fluctuate unnoticed, often requiring rework or even product disposal.
Flir thermal cameras and smart sensors provide continuous, non-contact temperature monitoring across the entire line. Instead of checking single points, operators can see the full thermal picture in real time. This allows teams to:
With industrial-grade resolution and ±2°C accuracy, thermal imaging supports confident, real-time decisions without interrupting throughput.
Manual sampling consumes labour and introduces variability. By integrating thermal imaging directly into HMI and SCADA systems, manufacturers can move to continuous monitoring rather than periodic sampling. Temperature data becomes part of the wider control system, not a separate manual task.
At one facility, 30-minute manual checks were replaced with round-the-clock monitoring using the Flir A70 Compact Smart Sensor Thermal Camera. The results:
Automation does not replace expertise. It empowers teams with the insight to intervene early, improving both safety and operational performance.
See all of our Food & Beverage Manufacturing Solutions
Food processing facilities are demanding: high heat, washdowns, tight spaces, and constant movement. Any technology needs to work within that reality.
The Flir A70 integrates with standard industrial protocols and connect directly to MES, SCADA, and plant networks. Data flows into dashboards and reporting tools already in use, and on-edge analysis provides instant verification without slowing output or adding infrastructure complexity, strengthening visibility and process control.

Temperature deviations carry real operational consequences: rejected product, rework, line stoppages and compliance investigations. Continuous thermal monitoring reduces these risks by spotting deviations early, before they affect large volumes. The benefits are clear:
Temperature is more than a number. It is a critical control variable. Real-time thermal and visual imaging replaces intermittent checks with continuous verification, providing traceability, documentation and confidence across every stage of production.
When you can see the heat clearly, you can manage risk proactively rather than reactively. In today's fast-paced food and beverage sector, that visibility is operational protection, not a luxury.
Preventing thermal variation protects product, revenue and brand integrity, but more importantly, it protects people.