Preventing Packaging Defects in Food & Beverage: How Thermal Inspection Protects Against Recall

In food and beverage manufacturing, packaging is more than a final step. It is the last line of defense. And that defense is under pressure.

Despite high-speed lines and advanced machinery, small defects still slip through. In 2024, food recalls increased by 10%, with faulty seals and underfilled packs among the leading causes. Meanwhile, up to 40% of seal defects go undetected in flexible packaging systems, and a third of global food waste is linked to packaging failures.

What appears to be a minor deviation on the line can escalate quickly: a weak seal, a micro-leak, an underfilled pack. Across thousands of units per hour, small faults multiply into waste, rework, complaints and sometimes full product withdrawals.

The financial impact is clear, and operational disruption is immediate, but the wider consequences often surface later.

The Real Cost of a Faulty Pack

Packaging failures do not always begin at the sealing jaw. They can stem from poor material compatibility, inconsistent temperatures, or design limitations that only reveal themselves under production pressure.

Weak or inconsistent seals and micro-leaks compromise product integrity. Each faulty pack represents lost product, wasted materials, and unrecoverable labour time. Energy has already been consumed. Ingredients have already been processed.

At scale, that waste erodes margin, and for businesses with ESG targets, packaging defects directly damage environmental performance. When a pack fails, both the packaging and the product inside are often discarded, undermining sustainability commitments as embedded carbon from sourcing, manufacturing and transport is lost. Sustainability targets become harder to achieve.

The human impact is just as real; production teams can feel the pressure when reject rates rise. Quality managers carry the burden during investigations. Retailers demand answers. Consumers lose confidence when a product does not meet expectations.

Preventing packaging defects is not only about quality control. It is about responsible manufacturing.


See all of our Food & Beverage Manufacturing Solutions


Building Visibility at the Point of Seal

Traditional inspection methods leave gaps. Manual checks and sampling cannot guarantee coverage at high speed. Thermal imaging provides a different level of visibility as seal integrity is fundamentally a thermal event. If heat distribution is inconsistent, the seal will be compromised even if it looks acceptable on the surface.

Systems such as the Flir A70 Fixed-Mount Thermal Camera monitor heat distribution during sealing in real time, helping operators maintain consistent seal quality through improved inspection insights, while introducing a deeper layer of control. Weak seals, voids, trapped contamination, and underfills are identified immediately.

The business impact is measurable:

  • Reduced product giveaway and scrap
  • Fewer seal-related rejects
  • Lower rework and downtime
  • Stronger process control and audit readiness

Quality shifts from reactive investigation to proactive control.

From Packaging Risk to Operational Control

When seal performance is verified in real time, fewer packs fail, and less product is discarded. Operational confidence improves because teams can see exactly what is happening at the point of seal.

Preventing packaging defects is not simply about avoiding recalls. It's about protecting yield, reducing waste, supporting sustainability objectives and giving people the tools to deliver consistent quality without uncertainty.

Technology enables visibility. Control enables stability. And stability protects more than product.

At the packaging stage, prevention strengthens operational resilience, safeguards performance, and ensures that every pack leaving the facility meets the standard your brand promises.

Explore how packaging defects can be identified earlier and prevented across your facility.

Back to top