Teledyne FLIR announces new G-Series Optical Gas Imaging Cameras


FLIR has been the leader in Optical Gas Imaging for years. And now, with the launch of the FLIR G-Series Optical Gas Imaging cameras, it has set a new standard in OGI, thanks to you.
The FLIR team spent years talking to customers, taking notes, and listening to feedback from operators and end users to learn how its OGI cameras could be improved and what needed to be done to ensure it was creating the most efficient camera for the Optical Gas Imaging customer.
With that feedback, FLIR developed a camera that has improved software integration for recording and reporting findings, better ergonomics that allow the user to more comfortably interact with the camera, and superior gas visualization and detection including the first ever in-camera gas quantification for the Gx320, G620, and Gx620 cameras.
No, it's capacitive touch. All buttons can be reached with joystick just like on the GF77 and FLIR premium handheld cameras.
No, the FLIR G-Series features new batteries and are not they are not cross compatible with the legacy FLIR OGI cameras. The run time is 2.5 hours with a charge time of 2 hours. Two batteries are supplied with the camera and additional are available for purchase.
The visual camera has been upgraded to a 5MP camera, which saves images in the resolution 1280 × 960.
Yes. The Gx320 has radiometric capabilities and image capturing capabilities.
The Gx320 and Gx620 cameras will be ATEX, IECEx, and HAZLOC certified for use in hazardous locations. These certifications will be downloadable on FLIR's support website (support.flir.com) as soon as they are available.
We have addressed this issue on the G-series by adding more lossless compression to .mpeg recording.
With OGI cameras (and IR cameras in general), a lower resolution camera of the same type will have better thermal (and gas) sensitivity. This means that a 320 × 240 camera will be able to see the smallest of leaks better but the difference is minimal and both cameras meet U.S. EPA sensitivity requirements (OOOOa & Appendix K). If your application is close range with the desire to see the smallest of leaks, the Gx320 camera will be the best on the market. If your general application is to view components from a greater distance and the smallest leaks are not as important, a Gx620 camera is recommended.
We will have 25°, 14.5° and 6° FOV lenses with the G Series. These are not compatible with legacy FLIR OGI cameras.
Yes, but the camera does not have a built-in microphone due to cooler making noise. Voice recording is available through Bluetooth® headset connected to the camera.
The GF309 camera has not changed and there is no update to the furnace inspection cameras at this time.
No, sketch is only possible on images and not videos.
There is space under the camera to fit the neck strap when attached to camera.
There is an extra slot to fit additional lenses in the re-engineered camera case.
Like all OGI cameras, the distance in which the camera can be used is dependent on the size of the leak being imaged. If using the FOV6 lens, you can image a leak at four times further than with a standard lens.
No, it’s a standard size.
The camera will have the same standard units of quantification as the FLIR QL320, which are standard in the industry. These will include a variety of mass and volume flow measurements as well as concentration-pathlength.
Quantification in Camera is unique and will work similar to the existing FLIR Q-Mode feature except that after the recording, you will immediately get a quantification reading (instead of the requirement to remove the SD card, put it in the QL320, process the file, etc. like with the current Q-Mode feature). A QL320 is not required for quantification but could be beneficial for some advanced users and additional features (like masking or sensitivity adjustment).
No. You can only quantify in IR mode as radiometric info in image is needed. You can use the camera in either auto or manual IR mode, which will allow other advanced features like 1-Touch Level/Span.
Quantification in Camera uses the same list of common gases (seven in total) as the QL320 as the predominant gas in the mixture. If there are multiple gases in the mixture, FLIR has a spreadsheet to assist in exact quantification readings. Using the predominant gas is recommended in all cases.
FLIR does not have a published quantification accuracy specification for our QL320 or quantification in camera due to the challenges in quantifying a turbulent gas leak with natural fluctuations in movement that continually changes. Instead, we prefer to point users to 3rd party evaluations of our solution like CONCAWE and the AMFC. In these studies, it was determined that on a single reading basis, there was error with the FLIR QOGI solution but when used in aggregate reading situations (averaging multiple readings), the technology was very reliable with error percentages of 6% and 18%, respectively.
Not yet. We hope to have full training videos soon on many features of the G-Series cameras, including Quantification in Camera.
To our knowledge, there is not an update regarding the U.S. EPA's acceptance of QOGI as an acceptable quantification technology. To the EPA, if an OGI camera finds a leak, it is required to be fixed and quantification is not necessary.
Yes. The G-Series cameras will meet EPA OOOOa and Appendix K gas sensitivity requirements the same as the GF Series. The detector in the cameras has not changed so the camera's capabilities related to gas detection have not changed.
No. Ignite™ is only available on the GF77 and G-series.
Users will get 1 GB of free storage for FLIR Ignite™ but additional storage in a subscription based model is available.
The camera has Wi-Fi and can connect directly to a device by using the camera as a "hotspot" or connecting the camera to another device that is set up as a "hotspot". While directly connected, you can stream an image or have remote control of the camera via the connected device. You can also use internet Wi-Fi with FLIR Ignite™ to upload images or videos. If a connection is good, 10m is likely an acceptable distance to directly connect to a device.