Unifying Disconnected Data: When Thermal and Visual Insights Work Together in Materials Science

Materials research often relies on multiple sensing systems. A thermal camera captures temperature and energy flow. A visible camera records structural changes, deformation, or fracture events. Traditionally, these datasets are collected separately, then painstakingly aligned during post-processing.

This workflow introduces risk: spatial misalignment, timing offsets, and data handling errors can compromise results and consume valuable research time. 

A Unified Approach with Flir Mix 

The Flir Mix multispectral imaging solution was developed to remove that burden. By synchronizing high-speed thermal and visible imagery into a single system and software environment, Flir Mix delivers spatially and temporally aligned data, pixel by pixel, frame by frame.

“With Flir Mix, we take the workflow off the researcher,” says Jerry Beeney, Global Director of Business Development at Teledyne Flir. “The infrared and visible data are aligned effortlessly, both spatially and in time. That’s critical for dynamic experiments.” 

Thermal, visual, and temporal data are aligned seamlessly without introducing the risk of error. 

Why Alignment Matters in Materials Science

In experiments such as tensile testing or fracture analysis, events happen quickly. The precise moment a crack initiates may coincide with a localized thermal spike. If visible and thermal frames are even slightly out of sync, critical insight can be lost.

Flir Mix ensures researchers see exactly what happened, when it happened, and where—without guesswork.

Enabling Repeatable, Defensible Research

Repeatability is central to academic research. Flir Mix supports this by allowing users to save experimental setups, analysis workflows, and visualization settings as reusable workspaces.

Researchers can:

  • Re-run experiments with identical parameters 
  • Share data and workflows with collaborators 
  • Support peer review with transparent, well-documented datasets

This consistency strengthens confidence not only within the lab, but also during publication and conference review.

Cracking the Code in Fracture Mechanics  

In a university materials lab studying fatigue and fracture behavior, researchers used Flir Mix to observe energy dissipation during cyclic loading of composite samples.

What changed with Flir Mix:

  • Thermal and visible data were captured simultaneously
  • The onset of fracture was identified earlier through localized heating
  • Data alignment time was eliminated
  • Results were easier to share and defend during peer review 

“Before Flir Mix, aligning thermal and visible data took hours and introduced uncertainty,” said Beeney. “Now the data is synchronized automatically, and our customers tell us they can trust what they’re seeing.” 

Accurate Data Is an Invaluable Investment 

While low-cost imaging options exist, in research, gathering reliable data matters. Using Flir Mix provides accurate, reliable data that is defensible. 
 
“If we say our system can do something, it does it,” Beeney explains. “That matters when someone’s research timeline or grant funding is on the line.” 

Flir Mix is part of a broader scientific imaging ecosystem designed for long-term academic research, supporting evolving experiments, growing teams, and increasingly complex datasets. 

Reducing Risk and Preserving Data Integrity

In university research, experiments are often expensive, time‑intensive, and difficult to repeat. When thermal and visual datasets must be exported, converted, and moved across multiple software tools, each handoff introduces risk: file corruption, version confusion, or subtle processing errors that may not be discovered until results are under review. A unified system like Flir Mix helps preserve data integrity by keeping thermal and visible information captured, stored, and analyzed together from the start. 

This matters not only for day‑to‑day analysis, but also for long‑term research programs where datasets may be revisited months or years later. Researchers retain access to the original, synchronized data along with the context needed to interpret it accurately, supporting transparency, reproducibility, and defensible conclusions throughout the research lifecycle. 

Designed for the Pace of Academic Research 

Flir Mix also reflects how academic labs actually operate: with rotating students, shared equipment, and evolving research questions. By simplifying setup and analysis, the system lowers the barrier for new users while allowing experienced researchers to scale experiments more efficiently. Less time spent aligning data or troubleshooting workflows means more time focused on discovery, interpretation, and publication.

For materials science and mechanical engineering departments balancing rigor, speed, and collaboration, this approach supports both immediate experimental insight and the long-term goals of funded, peer‑reviewed research—without adding complexity to already demanding workflows.

Want to know more?

A Breakthrough in Multispectral Infrared Imaging

Learn more about the Flir Mix 

Reach out to the Flir Science team to learn more about Mix  

Contact Us
 

 

정보 요청

Optin

제출할 경우 귀하는 Flir의 개인정보 보호정책 및 쿠키 정책에 동의하는 것으로 간주됩니다.

Back to top