Seeing the Invisible: A Better Approach to Emissions Detection in Downstream Operations

For refineries, petrochemical facilities, and storage terminals, fugitive emissions are more than an environmental concern. An undetected hydrocarbon or volatile organic compound (VOC) leak can mean lost product, additional maintenance, potential worker exposure, unplanned downtime, and increased regulatory risk.

Finding those emissions, however, can be challenging.

A typical downstream facility contains thousands of potential leak points across valves, flanges, compressors, pumps, storage tanks, piping systems, and other equipment. The scale and complexity of these environments can make conventional point-by-point inspection methods labor-intensive and time-consuming.

At the same time, regulatory requirements, methane-reduction initiatives, and environmental reporting expectations are putting greater emphasis on detecting and repairing emissions efficiently and documenting the results.

Optical gas imaging (OGI) gives operators another way to approach the challenge.

Turning Invisible Gas into Visible Information

FLIR OGI cameras use infrared imaging tuned to specific gas absorption wavelengths. Hydrocarbon gases absorb infrared radiation at certain wavelengths, allowing a properly configured camera to visualize gas as a moving plume against the background. Instead of determining the presence of gas one component at a time, an inspector can observe a larger area and identify the apparent source of an emission in real time.

 

This visual approach offers an important advantage in complex downstream environments. Inspectors can scan multiple components within a camera view and work from a practical distance rather than approaching every component with a probe. OGI can therefore complement existing LDAR programs while helping inspection teams increase coverage and focus attention where it is needed most. 

Where OGI fits into downstream operations

OGI can support several different inspection and maintenance activities throughout a facility.

Routine LDAR inspections: Teams can examine valves, flanges, pumps, compressors, pressure-relief devices, and other potential leak sources as part of recurring inspection programs. The ability to scan groups of components can make OGI particularly useful where large numbers of components must be evaluated

Process units: OGI can be applied around equipment such as FCC units, hydrotreaters, reformers, and distillation columns, providing another way to evaluate complex operating areas for fugitive releases. 

Storage and transfer: Tank farms, loading racks, pipelines, and marine or rail terminals present additional opportunities for OGI, particularly where equipment is spread across a large or congested area. 

Turnarounds and maintenance: During shutdowns, startups, commissioning, and repair activities, OGI can help teams identify unexpected releases, troubleshoot equipment, and visually verify repairs. 

Upset conditions: When abnormal operating conditions occur, seeing the location and movement of an emission may help teams assess the situation and focus response activity while maintaining distance from the suspected release 

Moving Beyond Point-by-Point Detection

Traditional inspection technologies continue to play important roles in emissions programs, but they can have practical limitations.

Portable gas detectors and flame ionization methods generally require the inspector to approach individual components. Soap-bubble testing can become impractical across large numbers of components. Fixed sensors provide continuous information at their installed locations but do not offer the mobility of a handheld inspection tool. 

OGI provides a complementary capability: wide-area, non-contact visualization.

An inspector can see the movement of a gas plume and use the image to help determine its source. That can help maintenance teams prioritize their response rather than simply knowing that gas is present somewhere in an area.

From Detection to Better Emissions Management

The value of OGI extends beyond finding a leak.

Earlier identification can enable earlier repair, helping reduce unnecessary product loss and fugitive emissions. Remote visualization can help inspection personnel evaluate difficult-to-access or potentially hazardous equipment without immediately approaching the suspected source. Images and recordings can also provide useful documentation for LDAR records, repair verification, reporting, and communication between environmental, operations, and maintenance teams. 

For facilities looking to build more comprehensive emissions-management programs, OGI can include complementary technologies such as quantification tools and fixed monitoring systems. The original downstream strategy identifies continuous emissions monitoring, AI-assisted leak detection, quantitative reporting, and connected inspection workflows as important directions for the technology.

FLIR OGI vs. Traditional Detection Methods

Method Limitations FLIR OGI Advantage
Portable gas detectors Point-by-point measurement Wide-area scanning
Soap bubble testing Time-consuming, impracical at scale Immediate visualization
Fixed Sensors Limited coverage Mobile, flexible deployment
Flame ionization Requires close proximity remote, non-contact inspection

 

Choosing the Right FLIR OGI Solution

FLIR offers several OGI options for downstream applications. The FLIR Gx320, G620, and Gx620 provide advanced gas visualization, sensitivity, and workflow capabilities for detecting methane, hydrocarbons, and VOC emissions across refineries, petrochemical facilities, storage and transfer operations, and other downstream environments. These G-Series cameras also offer in-camera gas quantification, helping operators estimate leak size and severity while supporting more efficient inspection, documentation, and emissions-management workflows.

Operational Need FLIR OGI Benefit
Inspect complex equipment Scan multiple components and broad areas
Find the source of a release Visualize gas movement in real time
Reduce unnecessary exposure Inspect remotely without direct contact
Confirm corrective action Visually verify repairs
Support emissions programs Capture images, video, and inspection information

 

A More Visible Approach to Managing Emissions

As downstream operators balance regulatory requirements, emissions goals, safety, maintenance, and operational efficiency, visibility matters.

FLIR optical gas imaging turns otherwise invisible hydrocarbon and VOC emissions into information operators can see and act on. By integrating OGI into LDAR, maintenance, and emissions-management programs, facilities can find leaks faster, focus repair efforts, improve documentation, and gain a clearer picture of emissions across complex operations. 

Want to learn more? Download the white paper, Enhancing Emissions Detection & Operational Efficiency in Downstream Operations with FLIR Optical Gas Imaging, to explore OGI applications, benefits, and solutions for downstream facilities.

Download whitepaper

 

お問い合わせ

Optin

フォームを送信することにより、FLIRのプライバシーポリシーおよびクッキーポリシーに同意したものとみなされます。

コンタクト - 光学ガスイメージング

 

Back to top