EARLY FIRE DETECTION FOR ROOFTOP SOLAR PV

After a rooftop solar fire, the detection method that usually gets recommended is linear heat detection cable. On a smaller commercial roof that is fair advice. The cable is well understood, the install is straightforward, and the cost matches the asset being protected.

The recommendation gets harder to defend on a single-tenant distribution center pushing past 500 thousand square feet. A roof that size needs hundreds of thousands of feet of Linear Heat Detection (LHD). The cable jacket has to survive the entire solar lifecycle outdoors, exposed to UV, freeze-thaw, ponding water, and routine maintenance traffic. Published performance data for that duty cycle is thin. A short or damaged run leaves a section of the array unprotected, and the repair means a costly effort to replace cable. 

There is also a question of what the alarm actually tells you. LHD reports that part of the run got hot. It cannot determine exact incident location. The response options collapse to two: evacuate an operational facility, with the downtime cost that follows, or send someone onto the roof to look. Many facilities install cameras to verify alarms, which increases system cost to do work the detection layer cannot do on its own.

 

THERMAL IMAGING PROVEN FOR HOTSPOT DETECTION

 

The maintenance side of the business uses thermal cameras to inspect rooftop PV systems already. Drone surveys, handheld inspections by O&M technicians use handheld thermal imaging to find hot connectors, failed bypass diodes, and degraded strings before they cause real problems. The methodology is codified in IEC 62446-3:2017. Insurers ask to see the reports. 

From a fire detection standpoint, large scale thermal imaging will not monitor every connection point. It will, however, alert on small beginning fires with exact location and temperature data, allowing operators or first responders ample time to respond proportionately. This approach is acceptable since the roof membrane is fire resistant itself, and early detection provides time to react before a fire gets out of hand. The ability to remotely verify an alarm and determine action without stepping foot on the roof can mean the difference between evacuating a large distribution or shopping center at significant cost.  



          
     


A single Flir camera, mounted on a parapet or pole, actively monitors more than 10,000 square feet of array, or monitor out to 410 feet of distance. Every pixel reads temperature. User-defined regions of interest carry their own absolute and rate-of-rise thresholds. When the system alarms, operators see what triggered it on the same screen, which removes one of the structural problems with LHD: verification is built in.


BUILT FOR OUTDOOR SERVICE

 

Outdoor longevity is not a research question for thermal cameras. The A-Series platforms have been deployed for years in environments substantially harsher than a roof: ports, steel mills, refineries, and outdoor BESS installations. NFPA 72, 2025 edition, recognizes thermal image fire detection as a prescriptive method in Section 17.12, which gives designers and authorities having jurisdiction, a defined basis to specify it within the fire alarm system. 

 

   

WHERE THIS FITS

 

  • Distribution centers, warehouses, and logistics hubs with continuous rooftop PV
  • Manufacturing, food processing, and cold-storage facilities
  • Data center campuses and other mission-critical buildings with rooftop PV
  • Retail, big-box, and supermarket roofs with carport or canopy arrays
  • Municipal, school, campus, and multifamily rooftops 

 

 

THE FLIR EARLY FIRE DETECTION SYSTEM

 

Flir A70 Advanced Multispectral Early Fire Detector (EFD) cameras combine a calibrated radiometric thermal sensor with a visible camera in one fixed outdoor unit. Three lens options (29°, 51°, 95°) match the camera to roof geometry, from long rows of modules to wider canopy spans. Each camera signals alarms through physical outputs to the fire alarm system and video + alarms via the facility's monitoring platform. 

 

CLOSING THE FEEDBACK LOOP

 

Thermal imaging technology is mature and the deployment story is proven. What is still developing is the conversation between site owners asking for better large-area outdoor detection and the Fire & Life Safety professionals writing the protection strategies. Multi-layered design remains the right approach for rooftop PV. The case here is for adding a fixed thermal layer to that design, alongside or in place of LHD where the site's scale, environment, or operational profile warrants it.

情報をリクエスト

Optin

送信することにより、フリアーシステムズのプライバシーポリシーおよびクッキーポリシーに同意したものとみなされます。

Back to top