Looking to add a moisture meter to your tool bag? Here’s what you need to know to find the right tool for you.

Moisture meters come in two varieties: pin and pinless. A pin moisture meter can provide quantifiable results but needs to pierce the surface to take measurements; a pinless moisture meter is faster and non-destructive, but only provides a relative reading.

Pin Moisture Meters

Pin moisture measurement requires the physical insertion of the two pin probes into the wall (or material in question). Then an electrical current is run between the two probes, and the material’s moisture content is determined by measuring the resistance the current encounters. Water, with its dissolved salts and impurities, conducts electricity while building materials such as wood do not, meaning dry walls and floors offer more resistance. The wetter the material, the more conductive it is.

MR55-bathroom-under-sink-JPEG-(Web---72-dpi).jpg

Because pin meters are sensitive to temperature and the type of material being measured, a good meter should come with options to compensate for the temperature and material encountered. The FLIR MR55, for instance, comes with a built-in library of 11 different material groups and automatically compensates for ambient temperature.

The takeaway: pin moisture meters provide you with a quantifiable measurement of the percentage of moisture in a material, but require some damage to the material being measured.

Browse all moisture meters

Pinless Moisture Meters

The advantage of pinless moisture meters is they won't damage your walls—but there's a catch. A pinless meter is a “relative” or unitless measurement device. Unlike a pin moisture meter that measures resistance, the pinless meter measures an electrical property of the material called relative permittivity.

To fully understand this measurement, it needs to be compared to a known dry sample of the same material. The best way to use a pinless meter is to make a measurement of a material of a known dryness, then make a measurement of an item of the same material, thickness, and construction.

Any rise in reading indicates moisture, or the presence of some other conductor or high permittivity material (a metal stud behind the wall, for instance, would produce high readings). Because of this, taking multiple measurements over the suspected area is highly recommended.

MR160_wall-JPEG (Web - 72 dpi).jpg

Pinless moisture meters may have a flat sensor that needs to be placed flush against the surface of the material, or may have a ball probe like the FLIR MR59 that allows you to easily measure into corners and around baseboards.

If you think you need both a pin and pinless moisture meter for your work, then the FLIR MR60 provides both an integrated pinless sensor and an external pin probe.

Infrared Guided Measurement

Another feature you may want to consider on a moisture meter is thermal imaging. FLIR meters equipped with Infrared Guided Measurement (IGM) use thermal imaging to help quickly locate potential moisture issues. Instead of hunting around for hidden leaks or signs of moisture, you can scan large areas to visually target the problem and then either verify it using the built-in pinless meter or an accessory pin probe. Learn more about detecting moisture issues using thermal imaging:

Moisture meters with IGM include the FLIR MR277, the MR176, and the MR160.

Browse all moisture meters

Artículos relacionados

Procedimiento

Historic Hurricane Season Highlights Need for Moisture Detection

Read more
Conceptos fundamentales

Consejos sobre cámaras termográficas para evitar errores en inspecciones rutinarias domésticas

Read more
Procedimiento

¿Cómo puede saberse si en su casa hay carencias de aislamiento?

Read more
Back to top