The Next Evolution of Autonomous Gas Detection Is Here
Introducing The New FLIR ADGiLE™ Gas Solution
By Stephen Beynon, Director of EMEA Sales, Optical Gas Imaging, Teledyne FLIR

By Stephen Beynon, Director of EMEA Sales, Optical Gas Imaging, Teledyne FLIR

Detecting gas emissions across complex industrial facilities presents an ongoing challenge: leaks can occur intermittently, equipment may be distributed across large areas, and different gases require different detection technologies. For operators, maintaining visibility across these environments is essential to effective emissions management.
For more than two decades, FLIR has advanced optical gas imaging (OGI) technology, helping oil and gas professionals visualize emissions that would otherwise be invisible. Building on the 2024 introduction of ADGiLE™ (Autonomous Detection of Gas Leaks and Emissions), FLIR is now expanding its autonomous gas monitoring solution to address a broader range of industrial applications.
Now, FLIR is taking the next step in that evolution.

The new ADGiLE monitoring solution is not simply an updated camera or methane detection system. It has evolved into a configurable, continuous emissions monitoring platform designed around the realities of industrial sites. The platform brings OGI hardware, intelligent analytics, remote monitoring, alarming, and workflow management together as a scalable monitoring solution.
It starts with broader gas detection. The original ADGiLE solution was focused on methane. The updated platform expands those capabilities with a choice of OGI technologies for applications ranging from methane to hydrocarbons to volatile organic compounds (VOCs), and with a new HR camera model, adds gases such as ethylene and ammonia. This gives operators greater flexibility to match their monitoring technology to the gases and applications that matter at their facilities.
That flexibility extends to the cameras themselves. ADGiLE can be configured with cooled or uncooled OGI technology, with multiple lens options available depending on the configuration and monitoring requirements.
Installation is flexible, too. Different sites present very different monitoring challenges. ADGiLE addresses this through fixed and pan-tilt configurations as well as hazardous-area (ATEX) and non-hazardous-area enclosure options. Pan-tilt capability can extend monitoring across multiple areas and equipment, helping facilities establish visibility across larger or more complex installations.
Most importantly, it’s more than a camera. ADGiLE combines imaging hardware with analytics, processing, connectivity, and application software in one continuous monitoring workflow. The automated system allows operators to review event information, recordings, and alerts remotely rather than treating detection as an isolated camera function.
Continuous monitoring helps operators identify intermittent emissions that periodic inspections may miss. Emissions are not necessarily continuous themselves; intermittent leaks and emissions events can occur between scheduled inspections. ADGiLE provides day-and-night continuous monitoring, helping operators identify those events and gain greater situational awareness across their facilities.
Visual confirmation adds context. Detecting an incident is only the beginning. OGI allows operators to see an emissions event, while ADGiLE's analytics and monitoring workflow are designed to help distinguish leaks from normal operational emissions and provide information that can help teams prioritize their response.
A key part of this evolution is an expanded choice of OGI cameras and deployment options. These options include:
Together, these capabilities move ADGiLE from a standalone product toward what we believe continuous emissions monitoring should become: a configurable solution built around the facility, the gas of interest, the monitoring area, and the installation requirements.
As industrial facilities seek greater visibility into gas emissions, monitoring solutions must adapt to different gases, equipment configurations and operating environments.
With expanded camera options, configurable deployment and integrated monitoring capabilities, ADGiLE represents another step toward more flexible, autonomous emissions monitoring.
At ADIPEC, we invite you to come see that future for yourself. Visit the Teledyne FLIR booth #9413 and talk with our gas detection experts about how ADGiLE can help move your operation toward the future of autonomous gas detection.
Learn more at: www.flir.com/ADGiLE