Smarter Predictive Maintenance in Cement Plants with Acoustic Imaging

Flir acoustic imaging cameras uncover hidden leaks and inefficiencies in cement plants, helping teams reduce downtime, cut energy costs, and boost performance. With intuitive operation, precise leak detection—even in noisy or hard-to-reach areas—and smart reporting, maintenance becomes faster, safer, and more cost-effective than ever.

The Challenge of Maintenance in a Growing Cement Industry

The global cement market was valued at $361 billion in 2024 and is forecast to grow at a CAGR of 5.1% through 2025–2032. Rising demand for residential construction, particularly in Asia, has driven production from 600 million metric tons at the turn of the century to over 2 billion metric tons in 2023—a staggering increase in global demand.

With such rapid growth, unscheduled downtime is a major concern in the quarrying and cement industry. Maintenance was once viewed as a cost center, often limited to annual shutdowns and reactive repairs. Today, however, leading operators recognize that regular scheduled maintenance is essential for boosting profit margins. In a typical 1-million-metric-ton-per-year plant, a single day of unplanned shutdown can cost up to $300,000.

Predictive and Preventive Maintenance in Cement Plants

Implementing predictive and preventive maintenance in cement plants is now a key strategy for maintaining uptime and ensuring equipment reliability. Advanced inspection tools like the Flir Si2-LD acoustic camera make cement equipment monitoring more accurate and efficient than ever.

By detecting small, compressed air or gas leaks before they lead to costly failures, acoustic imaging helps maintenance teams plan repairs proactively, avoid energy losses, and extend the lifespan of critical equipment. This proactive approach supports predictive maintenance programs, enabling cement producers to transition from reactive to condition-based maintenance with measurable ROI.

Precision Leak Detection for Predictive Maintenance in Cement Plants

A maintenance manager inspecting a plant with the Flir acoustic imaging camera

A maintenance manager inspecting a plant with the Flir acoustic imaging camera

Regular maintenance does more than prevent catastrophic failure. Hidden inefficiencies in plant and machinery can persist for months or even years, quietly eroding profits and competitiveness. The challenge is identifying these issues—especially in high-energy systems like compressed air and industrial gases, where leaks are often small, hidden, or obscured for operational reasons.

It is for this reason that Flir has developed the Si2-LD handheld acoustic camera. Equipped with highly sensitive MEMS microphones, the camera pinpoints leaks in compressed air systems while displaying a 12 MP image on a 5-inch, 1280 × 720 color screen. For noisy environments, the camera’s bandpass filtering allows users to isolate leaks with precision by manually selecting the frequency range, even in challenging industrial settings.

The Si2-LD detects sounds from 2–130 kHz, identifying even the smallest leaks. For example, a leak as tiny as 0.007 liters per minute can be detected from 2.5 meters away, and larger leaks can be located from up to 130 meters. This allows maintenance teams to safely inspect hard-to-access areas, including high-temperature zones, without risking personnel safety.

Cement Equipment Monitoring Made Simple with Flir Si2-LD

Once an inspection is complete, the camera’s onboard leak size quantification software helps prioritize repairs by potential energy loss, ensuring the most significant leaks are addressed first. Recognizing that plant environments often restrict external drives and Wi-Fi access, Flir provides a data cable accessory that connects the camera directly to a PC or laptop, allowing easy transfer of image files without network or security issues.

Engineers have also emphasized ease of use, noting that they often lack the time to become experts on every new piece of analytical equipment. Flir has designed the Si2-LD to be intuitive: a simple ‘point-and-shoot' operation handles detection, quantification, and analysis with minimal training required. The handheld device comes with a rugged carrying case to protect it in harsh environments such as quarries and cement works.

Smarter, Safer, and More Sustainable Operations

By integrating acoustic imaging into their predictive maintenance and cement equipment monitoring programs, cement manufacturers can achieve measurable reductions in downtime and energy waste. Detecting compressed air leaks early not only prevents unexpected failures but also contributes to sustainability goals by reducing emissions and overall energy use.

Request a Demonstration

For more information or an on-site demonstration of the Flir Si2-LD acoustic camera, please complete the contact form below. 

情報をリクエスト

Optin

フォームを送信することにより、FLIRのプライバシーポリシーおよびクッキーポリシーに同意したものとみなされます。

SEE IT IN ACTION

Book a demo today

Flir Si-Series cameras combine advanced acoustic imaging, intelligent analysis and intuitive workflows to make it easier to detect air and gas leaks, locate partial discharge faults and prioritize maintenance actions.

Industry-leading acoustic imaging cameras
Improving operational efficiency, asset reliability and performance
Trusted by professionals, proven in the field
Back to top