Finding Vacuum, Air, & Gas Leaks Faster in Semiconductor Manufacturing


Semiconductor manufacturing depends on tightly controlled production equipment and utility infrastructure. Compressed Dry Air (CDA), nitrogen and other specialty-gas distribution, pneumatic controls and vacuum-related systems are used throughout fab and subfab environments. With many valves, fittings, regulators, manifolds and connection points, small leaks can be difficult to locate quickly during routine inspection.
Undetected leaks can contribute to unnecessary utility consumption, higher operating cost and additional maintenance effort. In vacuum-related systems, unwanted leakage may also become an equipment or process concern. Efficient leak detection helps maintenance teams in their everyday work and minimizes disruption to normal operations.
Semiconductor fabs rely on extensive compressed dry air, nitrogen, specialty-gas, vacuum-related, and pneumatic systems. Timely leak detection can help reduce utility losses, improve maintenanceproductivity and support reliable fab operations.

Traditional leak inspections can be time-consuming when technicians must inspect large areas, trace long piping or work around packed equipment. In a fab or subfab environment, the challenge is localizing the source quickly enough to prioritize the right follow-up or repair action. Acoustic imaging visualizes the sound generated by a leak, helping technicians scan multiple potential leak points fast and efficiently.
Flir Si2-LD is an industrial acoustic imaging camera for pressurized leak detection and mechanical fault detection. In semiconductor manufacturing, it can support inspection of CDA systems, nitrogen and specialty-gas distribution, gas cabinets, valve manifolds, pneumatic controls, vacuum-related systems and other utility infrastructure where leaks could potentially happen. Rather than checking components thoroughly and one by one, technicians can scan large areas scan large areas, quickly locate leaks, capture snapshots for reporting, and move on to the required maintenance actions. Gases such as nitrogen, ammonia, helium, and argon are supported for estimated leak-rate and cost quantification. Si2-LD is also an efficient solution for vacuum leak detection.

Acoustic imaging should be used as part of the site’s established inspection and maintenance process. Access rules, cleanroom requirements, safety procedures, operating conditions and the characteristics of the target system should be considered before inspection. Detectability depends on leak size, pressure, distance, background noise and other site conditions. Findings should be reported and followed by actions according to facility procedures and approved equipment capabilities.