When QuickReport or any other FLIR software that requires camera connection installs, it creates a directory in the following location: C:\Program Files\FLIR Systems\FLIR Device drivers. All the drivers required for USB and Firewire cameras are in this location. They can also be found on the Software distribution CD.
Download the latest camera drivers
FLIR Device Drivers x86 (32-Bit)
FLIR Camera Device Drivers are all the drivers
for the FLIR Cameras for 32-Bit OS
Download and unzip before running the .msi file
FLIR Device Drivers x86.zip (775 Kb)
FLIR Device Drivers x64 (64-bit)
FLIR Camera Device Drivers are all the drivers
for the FLIR Cameras for 64-bit OS.
Download and unzip before running the .msi file
FLIR Device Drivers x64.zip (984.1 Kb)