What Are the Inherent Risks of BESS Sites, and How Can Operators Overcome Them?

Battery Energy Storage Systems (BESS) are revolutionizing the way we power our world, acting as the source that keeps renewable energy flowing even when the sun isn’t shining or the wind isn’t blowing. 

As the backbone of modern energy infrastructure, BESS plays a crucial role in balancing supply and demand. However, with the increasing adoption of large-scale battery storage comes the responsibility for manufacturers, site managers and regulators to manage its risks effectively.

The High-Voltage Threat: Thermal runaway in battery storage

Thermal runaway is the equivalent of a system overload. It’s a dangerous chain reaction in which an overheated battery cell loses its stability and begins to ignite its neighbors, setting off a firestorm that’s incredibly difficult to contain. It's of particular concern when dealing with lithium-ion batteries used in products such as electric vehicles, portable electronics, and grid-scale storage.

ev battery multi cells.jpg

Much like an electrical surge that fries a circuit, thermal runaway rapidly escalates, putting lives, infrastructure, and energy security at risk.

Several factors can cause this dangerous phenomenon to ignite, including:

  • Overcharging or overdischarging: Pushing a battery beyond its limits can cause excessive heat buildup, leading to system failure.
  • Physical damage or manufacturing defects: Cracks, punctures, or design flaws can create weak links in the chain, making failures more likely.
  • Environmental conditions: Exposure to high temperatures or external heat sources can turn a stable BESS into a ticking time bomb.

The fallout from a BESS fire can be severe, resulting in massive financial losses, grid instability, and environmental harm. And when you consider that these storage units are often installed near other high-energy infrastructure, the potential for disaster multiplies.

With the adoption of BESS units ramping up across the globe, soaring by more than 50% in 2024* alone, the potential risks must be managed in a way that safeguards workers, critical assets, communities, and the environment.

Stop the Spark Before it Starts: The power of thermal monitoring

The best way to prevent thermal runaway is to detect heat anomalies before they escalate. But without the right monitoring tools in place, operators are left in the dark, often unaware of hidden dangers until it’s too late.

That’s where thermal imaging technology plays a pivotal role. By offering continuous, real-time temperature surveillance, advanced thermal imaging can alert personnel to dangerous situations as they being to develop, so that no hot spot beyond specifications goes unnoticed. Like a circuit breaker that prevents an electrical overload, thermal monitoring acts as a failsafe, allowing site managers to catch and address overheating batteries before they ignite.

Energizing Safety: What makes a  strong thermal monitoring system?

To truly keep BESS operations running smoothly without the risk of meltdown, thermal monitoring systems must offer:

  • High-resolution imaging: The ability to detect even the slightest temperature variations across battery stacks, ensuring no heat anomaly slips through the cracks
  • Wide field of view: Comprehensive coverage that leaves no blind spots, just as a well-designed electrical grid leaves no home without power
  • Advanced analytics: Smart detection technology that filters out false alarms caused by reflections, weather, or routine human activity
  • 24/7 real-time monitoring: A non-stop watchdog that never sleeps, ensuring site managers stay wired into potential risks at all hours.

With 640 × 480 thermal resolution, FSX® (Flexible Scene Enhancement) technology, on-the-edge analytics, and offered fields of view up to 80°, Flir’s industry-leading A500f/A700f Advanced Smart Sensor camera is key to ensuring site owners' valuable peace of mind. 

A500f-A700F-3qtrFrtRght-01.png

The Flir A500f/A700f Advanced Smart Sensor

Site owners can also take advantage of the Flir FH-Series R Multispectral Camera featuring onboard, noncontact temperature measurement capabilities for fire detection, safety, and thermal monitoring of valuable equipment, plus 4K visual camera and easy VMS integration. The onboard radiometry in the camera, combined with Pan-Tilt-Zoom capability, enables continuous wide area coverage and round the clock monitoring against potential fires. When a hot spot or surface temperature change is detected, the contactless temperature measurement can be sent to an operator through a connected Video Management System (VMS) for instantaneous assessment and deployment of response tactics.

fh-series-r_smaller.png

Flir FH-Series R Multispectral Fixed Camera

Powering a Safer Future

BESS technology is charging ahead, and with it, the responsibility to keep energy storage systems safe and stable. If left unmonitored, thermal runaway could pull the plug on renewable energy progress, jeopardizing the benefits of grid resilience, sustainability, and energy security. 

By integrating cutting-edge thermal imaging into BESS infrastructure, operators can stay ahead of the curve, preventing small temperature fluctuations from sparking massive disasters. Because in the high-stakes world of energy storage, early detection isn’t just a bright idea—it’s the only way to keep the power on.

Learn more about solutions for early fire detection at BESS and other industrial sites here. 

 

*According to market intelligence firm Rho Motion

Back to top