I can't see the image stream in IR-monitor if I have userweb open. Why?

1. Open the A320 camera in the userweb

2. Connect A320 in the IR Monitor application

Result : The image stream will not appear in the IR Monitor application but the control will appear for that camera.

 

Here is a workaound for this behavior:

1. Connect A320 camera in the IR Monitor application

2. Open the same A320 camera in the userweb

Result : you will see the image stream and controls on both Userweb and IR Monitor

Back to top