Dport.exe should be there and it is not a virus. It is part of the Neevia DocCreator program that Reporter uses to create PDF files. A solution is to update your McAffe or to add an exclusion.
How to update your McAfee:
DAT files, engines need to be updated to include regular changes and improvements made to the scanner.
Engine and DAT updates are available at: http://www.mcafee.com/apps/downloads/security_updates/dat.asp
how to set exclusions:
1.Right-click the VirusScan Enterprise icon in the system tray and select VirusScan Console.
or
Select Start, Programs, McAfee, VirusScan Console.
2. Double-click On-AccessScanner.
3. Select All Processes.
4. Click the Detection tab.
5. Select Exclusions.
6. Select Add.
7. Add the relevant exclusion (FLIR SYSTEM folder).
8. Click OK three times to exit the On-Access Scanner.
9. Close the VirusScan Console screen.