The Create panorama image will usually work best if the images are taken at the same distance, with same focus and same zoom factor.
In order to create a panorama image a minimum of 30% overlap is required between consecutive images. Preferably, the images should be taken standing at the same position.