When I have too many measurement functions (boxes and spots), I cannot see them all in the RTSP stream. Can I solve this?

If you configure your FLIR AX8 using too many measurement functions, there is a risk that you will not have enough space to display all of them in the RTSP stream. The RTSP stream is shown in the image below, and it is evident that there are two measurement areas/boxes that are not visible because there is insufficient room for them.

This can be partially solved by hiding some of the information in the boxes. To do this, enter a box, as in the image below, and then change what you want to show (indicated in yellow).

Instructions

You could, for example, hide "Measure box max" from each area, thus making space to display other information in the boxes. However, if information is hidden, the alarms associated with them will be inactivated, and will need to be reactivated for them to work.

Back to top